STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MT35XU02GCBA2G12-0AUT compatibility with STM32N6 XSPI?

Hi everyone,Has anyone interfaced the Micron MT35XU02GCBA2G12-0AUT (2 Gbit xccela Flash) with the STM32N6 XSPI controller? I  would like to know if it works with the existing Macronix presets or needs custom XSPI settings.Any working example or exper...

GBA by Associate II
  • 378 Views
  • 1 replies
  • 0 kudos

STM32U083RC RTC wakeup mcu from stop mode

I have three questions regarding the STM32U083RC: 1.Why  is the reset value of EXTI_IMR1 register 0xFFF80000?The EXTI line 19-21 is configurable lines。 2.I encountered a problem: when I used the NUCLEO-U083RC demo program to PWR_STOP2_RTC, I found th...

clin.12 by Associate
  • 1021 Views
  • 2 replies
  • 0 kudos

Resolved! UART maximum tolerated deviation

So I am reading the RM0008 Reference manual because I need to describe some limits for my systemI am looking for the UARTs tolerance of clock drifton page 800 I am confused by these tables: In my case DIV_FRACTION is different from 0 and the M bit is...

NF is dont care.png
Moose by Associate II
  • 1036 Views
  • 3 replies
  • 1 kudos

STM32G4CET6 Boot0

Can I ask how to use my PB8 pin as CAN, since it is Boot 0? I pull Boot 0 to Ground to avoid it floating, then how to use it as CAN pin

ShiYi by Associate
  • 3181 Views
  • 2 replies
  • 0 kudos

Resolved! STM32N6 ITM console

Hello,I have custom board with STM32N6. I followed guidelines how to enable the ITM console:https://community.st.com/t5/stm32-mcus/using-the-itm-console-for-printf-redirects-and-lwip-debug/ta-p/723472The System Core Clock is set to 600MHz, confirmed ...

PeterPan by Associate II
  • 1030 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.