2025-10-13 5:01 AM - last edited on 2025-10-13 6:10 AM by KDJEM.1
Hi everyone,
Has anyone interfaced the Micron MT35XU02GCBA2G12-0AUT (2 Gbit xccela Flash) with the STM32N6 XSPI controller?
I would like to know if it works with the existing Macronix presets or needs custom XSPI settings.
Any working example or experience would help.
Thanks!
2025-10-13 6:09 AM
Hello @GBA ;
Could you please share the memory datasheet?
To check whether a device is supported by the XSPI interface, you need to refer to memory datasheet and the STM32N6 reference manual and precisely the command format and order.
The command format and order shared in the device datasheet must be aligned with the command format and order mentioned in the STM32 reference.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.