STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a way to change pins for FMC

I spent last 2 weeks trying to get 3.97inch 16BIT Module NT35510 to work with STM32L4S9ZIT6 I followed pin connection with diagram found somewhere. There is PIN CS on LCD with is connected to FMC_NE4. FMC_NE4 is kept high, while CS is LCD enable and ...

MNapi by Senior III
  • 1332 Views
  • 1 replies
  • 0 kudos

Resolved! Blink led problem

Hi everyone, I am starting to program a board with stm32 (stm32f103c8t6) and I have the following problem.I have two codes to make a led blink, but one works and the other doesn't work.Code 1 (not working)#include "stm32f1xx_hal.h" #define LED_PIN ...

CCuev.1 by Associate
  • 1996 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F722ZE SPI with DMA Reset question

I have a working, basic SPI transmit working with DMA. It transmits 20 characters in loopback mode and is working as it should. The GPIO Pins are set up correctly.SPI Configuration;void SPIInit() { RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; // Master SP...

MHank.1 by Associate III
  • 1672 Views
  • 1 replies
  • 0 kudos

dear support, when i use STLINK-UTILITY to change the option byte, it shows the error that "Read/Write protected zone for Bank 1 cant be reduced Please enter a correct value".

I want to change the boot0 configuration through stlink utility.so i set the option ​Bytes like the figure after connect to the board.but some error happened when i click the apply, like following does anybody know how the solve this problem, please ...

0693W00000aJqKyQAK.png 0693W00000aJqGJQA0.png
俊孙.1 by Associate
  • 1124 Views
  • 1 replies
  • 1 kudos

FOC inverter refrigerator compressor

HI all I work with compressor, I use ST MotorControl Workbench to debug, after configuring and pressing start motor after, my compressor has no response.Can anyone help me? :folded_hands: :folded_hands: :folded_hands:

0693W00000Y8IxXQAV.png
MMcAl.1 by Associate III
  • 3053 Views
  • 5 replies
  • 1 kudos

what is the limitation for buffer size in SAI DMA?

I am working on the STM32F769 series microcontroller in my project. I am using SAI interface of the mcu. And of course I also use DMA of SAI interface . I adjusted the DMA(DMA2 Stream 1) as listed below in the application :DMA Request Settings : Mode...

Resolved! My code is correct for push button ?

Thank you for helping and checking in advance:LED on and Off working well, without if codeI am using https://os.mbed.com/platforms/ST-Nucleo-L496ZG-P/#board-pinoutaccording https://www.st.com/resource/en/user_manual/um2179-stm32-nucleo144-boards-mb13...

CG3 by Associate III
  • 10191 Views
  • 6 replies
  • 0 kudos

Keil external download algorithm programming failed

The MCU is NUCLEO-H7A3ZI-Q, and I used OSPI to drive w25q128. It is known that it can read and write normally. Then, I modified the sct file in Keil and completed the FLM file. Erase can proceed normally, but an error was reported when the Program re...

_legacyfs_online_stmicro_images_0693W00000bhlBjQAI.png
fzhan.3 by Associate
  • 1190 Views
  • 1 replies
  • 0 kudos

STM32L431 strange current draw

I have made a small/simple circuit with an STM32L431, where I first made a prototype version on a breadboard and then had the same circuit manufactured on a custom PCB: The breadboard edition works exactly as expected. The PCB edition however is acti...

_legacyfs_online_stmicro_images_0693W00000bhkSAQAY.png _legacyfs_online_stmicro_images_0693W00000bhkS0QAI.png _legacyfs_online_stmicro_images_0693W00000bhkRqQAI.png
SKjær.1 by Associate II
  • 5139 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.