STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read Continuous Data from An the SPI interface

int main (){   uint16_t txConvertData[2]={0}; uint16_t rxConvertData[2]={0};   const uint16_t ConvertCommandMask = 0b0000000000000000;   while(1){ for (int j = 0; j < 2; j++) { // Send read command HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port,...

AE104 by Senior
  • 1441 Views
  • 2 replies
  • 0 kudos

What is proper way to resume DMA after waking up?

HiI searched everywhere but I'm stuck with starting DMA after waking up STM32L053C6U6 from stop mode. Chip displays LCD content, goes to sleep, wakes up by external interrupt on pin, receives SPI data through DMA,sends few bytes at the same time, upd...

I have to restart MCU to set RTC date in STM32F205ZG. I wrote a Set date and set time function for RTC. while Set time function updates the RTC time properly, set date function does not update the RTC date until I reset the MCU!

I am using STM32F205ZG RTC with External clock; the RTC initalization, RTC set Date function in the following lines:int16_t RTC_HAL_init(void){  RTC_InitTypeDef RTC_InitStruct;  /* Enable the PWR clock */  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, E...

MYahy.1 by Associate II
  • 4937 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G0 series Programmers & Debuggers

Hello All,I'm new to ST products. We are using STM32G041F8P6 in our project. This IC will be programmed through I2C/USART and there's no JTAG available for this chip. Please suggest some low-cost programmers/debuggers.Thank you

sagar_bn by Associate II
  • 3898 Views
  • 5 replies
  • 0 kudos

Resolved! Failure when Configuring UART2 in the STM32C031C6

When configuring UART2 in the STM32C0316-DK, the emulator is locked.Error in executing 'step' command ... Target is not responding, retrying...Code is running here (stm32c0xx_hal_msp.c line 272):  /**USART2 GPIO Configuration  PA8   ------> USART2_TX...

tpeng.1 by Associate III
  • 1945 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.