2023-04-10 12:57 AM
I am working on the STM32F769 series microcontroller in my project. I am using SAI interface of the mcu. And of course I also use DMA of SAI interface . I adjusted the DMA(DMA2 Stream 1) as listed below in the application :
DMA Request Settings :
Mode Circular, and increment address is memory as "half word"
And, I strongly wonder what is this limitations of DMA circular buffer? So, how many bytes can I kept inside the circular buffer?
2023-04-10 1:24 AM
You set up the number of *transfers* in given DMA Stream's NDTR register, which is 16-bits wide, so that's the buffer length limitation.
> So, how many bytes can I kept inside the circular buffer?
65535 * 1 or 2 or 4, depending on how do you set up PSIZE field in given stream's CR register.
Read the DMA chapter in RM.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.