STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Memory Device Compatibility Issue with STM32H47

Hi all,I hope everyone is progressing well with their projects.I'm currently working with the STM32H47 series microcontroller. In my project, I log certain values and store them in external flash memory. Later, I use USB host functionality to retriev...

Spinoza53 by Associate II
  • 1255 Views
  • 5 replies
  • 5 kudos

STM32 H757 DMA IRQ latency

Hello,I am using a STM32H757 to convert 12 analog channels using ADC2 and ADC3 (code running @ Cortex M7).- Both ADC are configured at 42MHz sync clock, triggered by a timer- ADC2 use DMA1s0 to transfert data to AXI SRAM.- ADC3 use DMA1s1 to transfer...

tarzan2 by Senior
  • 1011 Views
  • 4 replies
  • 1 kudos

Resolved! USB Device no recognized

I have diymore stm32f407vgt6 board , I connect usb  give DEVICE NOT RECOGNIZED  if i try DFU mode BOOT0 >3.3V, BOOT1 > GND, I try  every thing  but nothing . please  help mee

Resolved! STM32H563 clock at 250Mhz

I was trying to get the most out of my H563 set up and run as fast as possible. I am using the Nucleo-H563 board. I reconfigured in CubeMX to use System clock mux to use HSE source mux, multipliers and dividers set correctly for 250MHZ operation. The...

Resolved! Interfacing 32-bit SDRAM with STM32H750XBH6

Hello ST Support Team, I’m currently designing a custom board using STM32H750XBH6.In this design, I would like to interface a 32-bit SDRAM for improved memory bandwidth and performance. However, I noticed that in the official STM32H750 development bo...

Geethat by Associate III
  • 1229 Views
  • 3 replies
  • 5 kudos

Resolved! Inquiry about- DCMI of STM32U595RJT6Q

Good Evening Sir/Mam, Sir/Mam, I have a query about the DCMI of STM32U595RJT6Q. I have read the Datasheet of STM32U595xxx and it was written in it that- DCMI of this MCU is for use with Black & White Camera Modules and it is assumed that all preproce...

Ankur_1 by Associate II
  • 1466 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.