STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747BIT6 Not running code

I have been working recently on a board that i have made for a flight computer. But unfortunately, I have encountered some problems while programing the board.The conection to the board works great, and I´m able to upload de code and read it. The Iss...

Resolved! USBX MSC + FileX + NAND Flash - Windows I/O

Hello,I am building and application with a STM32U575 and a 4Gb NAND Flash. What I am trying to achieve now is to upload files from my PC through USB and then used these file within the STM32 using FileX.I already managed to set up FileX and LevelX to...

Pepils by Associate II
  • 13552 Views
  • 10 replies
  • 4 kudos

Resolved! STM32H7S7L8 dual USB

Hi ,I'm working on the STM32H7S7L8-DK and i would like to know if it is possible to use both USB_FS and USB_HS as two separate Virtual-port-com Device mode When I try to do it for one it is impossible in cube MX to do it for the other.Thanks !  

Hamady_1-1760681664387.png
Hamady by Senior
  • 831 Views
  • 8 replies
  • 0 kudos

Resolved! stm32h723zg Clause 45 MDIO

Hi all,i see H7 supports clause 45 MDIO access, but in the HAL library looks not implemented, i see only clause 22.How should i proceed to read/write c45 ? Thanks,angelo

heisenbug by Associate III
  • 4168 Views
  • 13 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.