STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can a camera be configured to read a QR code using stm32

I am using the Nucleo-L476RG board, and I am trying to configure the board to scan a QR code using a camera module. My question is, can I use a normal camera configured with the board and then code it to read QR codes, or do I need a specific QR read...

CDe S.2 by Associate
  • 2585 Views
  • 3 replies
  • 0 kudos

Counter Problem in Timer Interrupt

Hello,I set a timer timer in global interrupt mode. I monitored successfully a GPIO toggling with desired interrupt frequency. But a counter didn't increase in every timer interrupt cycle it was stuck at 1. Do you have any suggestions about the probl...

AE104 by Senior
  • 7915 Views
  • 27 replies
  • 0 kudos

STM32F722RE UART DMA RX not working properly

Hello all,I have an STM32F722RETx that is receiving data on UART from an ESP8266. This data is variable in length and I use DMA + IDLE interrupt to know when to process it. When debugging the code I can only see the first byte in the buffer as no oth...

Read and write TLE5012b registers with stm32g431

Hi. I'm new to st programming so I want to ask some questions. I'm trying to initialize an angle sensor TLE5012b on stm32g431 MCU but it seems that it has problems with writing and reeding registers. What I'm doing wrong?//spi initialization static v...

IKand.1 by Associate
  • 1486 Views
  • 0 replies
  • 0 kudos

Capture IRQ is called but interrupt flag is not set

We are using STM32G051 to measure duty cycle of the actuator PWM signal.TIM1 is configured in slave reset mode, with CH1 direct capture on rising edge and CH2 indirect capture on falling edge. Two DMA channels transfer results into two memory buffers...

maple by Associate II
  • 4606 Views
  • 5 replies
  • 0 kudos

Resolved! [Solved] STM32F4 I2C Master Clock Stretching Fail

Posted on September 26, 2017 at 02:56Hi there,I am attempting to get an STM32F411CE microcontroller to interface with a BNO055 IMU using the I2C peripheral. This particular IMU uses clock stretching which doesn't seem to work with the HAL_I2C librar...

0690X00000608QMQAY.png 0690X00000608N3QAI.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.