STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

receive data uart with DMA

I am trying to receive data over usart using dma with LL. I'm stuck with this for one week. I need help please.

LOnGr.1 by Associate III
  • 5225 Views
  • 11 replies
  • 0 kudos

Resolved! Error in AN2867 regarding oscillator choice?

Hello,I think I found an error in the AN2867 and just wanted to confirm it, before we hack around in hardware.We use an H7 with an external LSE. Fate landed us on the ABRACON ABS05-32.768kHz with 12.5pF. According to AN2867 it is suitable for the H7 ...

CSchw.4 by Associate
  • 1408 Views
  • 1 replies
  • 0 kudos

VSCode Extension for STM32Cube, import fails

I have a client project written using STM32CubeIDE. When I import the project into VSCode using the STM32 extension, the build fails because not all the include file paths were correctly imported.Sid

SidPrice by Associate III
  • 1301 Views
  • 1 replies
  • 0 kudos

Problem with standby mode on STM32l011K4T6

Hello everyone !I have a problem about low power mode on STM32. I use a STM32L011K4T that i soldered on a PCB. I want to use the standby mode with RTC.I used the example code from controllerstech website to try in a first place this mode and it was n...

FPOTH.1 by Associate
  • 2975 Views
  • 3 replies
  • 0 kudos

RTC not working correctly with octoSPI(stm32h723)

Hello everybody.I want to ask a question about a project. In my project, when octoSPI and RTC work together, an error occurs (counting incorrectly) in RTC's counting and it starts to count slower, but when I turn off octoSPI, RTC starts counting corr...

Mtopa.1 by Associate II
  • 1781 Views
  • 2 replies
  • 0 kudos

Resolved! Does the STM32G070CBT6 have a Unique ID?

In spite to the reference manual of the STM32G071CBT6 the unique ID is not described in the reference manual of the STM32G0x0 series, but its address is defined in the header file (stm32g070xx.h).Now I wonder if it is missing in the reference manual ...

stst9191 by Associate II
  • 3477 Views
  • 4 replies
  • 0 kudos

STM32H563RG internal flash memory Holding?

When reading the internal flash memory in the STM32H563RG MCU, there is a phenomenon that the core stops when reading 1 byte of sector 127 (0x080FE000) of 1 bank.When reading, it simply accesses the pointer and copies the data.*chBuf++ = *InternalFla...

YJin.11 by Associate
  • 1485 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.