STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Arbitrary waveform generation using timer DMA-burst feature: what is the callback when DMA transfer is complete/half complete?

I am expecting there must be a similar callback function like HAL_UART_TxCpltCallback, HAL_UART_TxHalfCpltCallback in case of using UARTs when using DMA-burst for generating arbitrary waveforms with PWM in order to be able to update the memory buffer...

nikwest by Associate II
  • 3778 Views
  • 6 replies
  • 0 kudos

With the canopen protocol I m unable to use more than 2 TPDO

Hello,When I m using more thant 2 TPDOs (configured with the OD_editor), the 2 first TPDOs are sent and then, nothing happens.In CO_CANsend I have the error CO_ERROR_TX_OVERFLOW. If i only use 2 TPDOs, it works perfectly.When i put a breakpoint befor...

AGiry.2 by Associate II
  • 2552 Views
  • 2 replies
  • 0 kudos

How the standard library runs in RAM

Hi.I am trying to run on RAM using STM32F407.How can I get the standard libraries (stdlib,stdio,string...) to run in RAM?​STM32F407VETX_FLASH.ld.data:{.....*libc.a:*(.text .text*).....}​statement was not allowed.​thank you

UpStream by Associate II
  • 812 Views
  • 0 replies
  • 0 kudos

Resolved! RTC drift

I am currently working on an RTOS application that includes RTC, and have observed that there is a clock drift of approx. 25 to 32 seconds after a 24-hour measurement cycle. Additionally, the drift seems to be not linear.I've measured the RTC frequen...

KIbra.3 by Associate II
  • 8694 Views
  • 6 replies
  • 0 kudos

SPI communication on STM32H7

SPI communication on STM32H7Working on interfacing Nucleo-H7A3 to COMX-CN-FB evaluation board which embedded netX made by Hischer using SPI interface.   Using SPL's SPI Transmit & Receive library, I implemented and proved the SPI data transmit & rece...

Resolved! LPUART missing first bit when using LSE, Works fine with HSI

We am using the Murata 1SJ which has a STM32L072CZ MCU and internal LSE, We trying to decode a UART stream from a Ublox GPS device using the LPUART in STOP mode. BAUD 9600 8 bits, 1 stop, no parity, all standard stuff.When i clock the LPUART with HSI...

JWieb by Associate III
  • 2940 Views
  • 4 replies
  • 1 kudos

how to capture pwm pulse width in stm32f103?

Hello, I'm already try this Input capture method for pwm pulse width. But frequency capture stored at a variable properly. And i need to capture pulse width too. but i try to capture pulse width and output has not given properly. and I'm change the ...

mrsmile by Associate III
  • 1070 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.