2023-04-13 1:11 AM
Hello everyone !
I have a problem about low power mode on STM32. I use a STM32L011K4T that i soldered on a PCB. I want to use the standby mode with RTC.
I used the example code from controllerstech website to try in a first place this mode and it was not working so i tried the example code from STM32Cube IDE (PWR_STANDBY_RTC) but it was the same.
The problem is, the MCU seems to go in standby mode (i use a x-nucleo-lpm01a to see the current) and i see a current of 260uA that seems the datasheet's value. After the wakeup, i see 5mA (that is not normal for me because when i try other program on the chip without low power mode, the MCU run at approximately 700uA with my clock) and that's all, the MCU stay blocked on the value of current and don't repeat the program as if there was an error in the reset.
I use the LSI clock at 37kHz and the HSI clock at 16Mhz that give a SYSCLK and HCLK at 2.097 MHz.
I only activate the "debug serial wire" and the "system wake up 1" on the SYS part of the ioc file.
Here is my code, thank you for your help.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
RTC_HandleTypeDef hrtc;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_RTC_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_RTC_Init();
/* USER CODE BEGIN 2 */
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // clear the flag
/** Disable the WWAKEUP PIN **/
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1); // disable PA0
/** Deactivate the RTC wakeup **/
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
}
/** Now enter the standby mode **/
/* Clear the WU FLAG */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* clear the RTC Wake UP (WU) flag */
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
/* Enable the WAKEUP PIN */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
/* enable the RTC Wakeup */
/* RTC Wake-up Interrupt Generation:
Wake-up Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI))
==> WakeUpCounter = Wake-up Time / Wake-up Time Base
To configure the wake up timer to 5s the WakeUpCounter is set to 0x2710:
RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
Wake-up Time Base = 16 /(37KHz) = 0.00043 seconds
==> WakeUpCounter = ~10s/0.00043s = 23255 = 0x2710
*/
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0x5AD7, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
/* Finally enter the standby mode */
HAL_PWR_EnterSTANDBYMode();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief RTC Initialization Function
* @param None
* @retval None
*/
static void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
/** Enable the WakeUp
*/
/*
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
*/
/* USER CODE BEGIN RTC_Init 2 */
/* USER CODE END RTC_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2023-04-13 1:38 AM
Hello @FPOTH.1 and welcome to the Community :) ;
Please check the parameters mentioned in the datasheet and precisely in table 30, 31 and 33.
Make sure that, if all free pins are set as analog.
For that I advise you to take a look at How to minimize the power consumption in low power mode: An example using NUCLEO-F401RE board article.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-13 1:58 AM
Thanks for your answer !
So i just tried and it still does not work :(
But my first problem is not the current consumption (i mean it's a problem but the main one is that the reset does not work as excepted).
Normally if i understood, when the MCU go in standby mode, everything is turn off except RTC and 2 wake up pins depending on configuration. And when the wakeup is triggered. The MCU is supposed to reset and start to read the code from the beggining. Is that right ?
But in my case, the MCU go in standby mode, after i have a wakeup from the RTC interrupt and ... nothing else. Like if when the reset occurs something go wrong and the code is not launch again.
2023-04-13 3:39 AM
Hello @FPOTH.1 ,
In the Standby mod, the VCORE domain is consequently powered off. The PLL, the MSI, the HSI16 oscillator and the HSE oscillator are also switched off. SRAM and register contents are lost except for the RTC registers, RTC backup registers and Standby circuitry.
and after waking up, program execution restarts in the same way as after a Reset (boot pins sampling, vector reset is fetched, etc.)
I recommend you this FAQ "How to configure the RTC to wake up the STM32 periodically from Low Power modes" , may help you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.