Ask questions, find answers, and share insights on STM32 products and their technical features.
I have an .elf file and a .mpa file both in the same directory, Debug-->project.elf and Debug-->project.map and the build analyzer is not showing any information. Any ideas on a possible solution to resolve this? SRM32 CubeIDE Version: 1.12.0
I looked at the pages for both MCUs side-by-side:https://www.st.com/en/microcontrollers-microprocessors/stm32f407ze.html/https://www.st.com/en/microcontrollers-microprocessors/stm32f407ve.htmlI can detect no difference other than the Z vs. V in the n...
Hi everyone,I am trying to get the SAI1 periperhal configured in I2S Standard mode going on the STM32H753ZI. During my testing sessions I found that my master clock is so far off it doesnt make sense. Based on the figure 652 within the TRM, it shows ...
I want to replace STM32L083RZH6 with STM32L083RZH3 and I suppose it's safe, but I cannot find information about the difference in the Datasheet.
NUCLEO-H723ZGI would like to have a triggered Arbitrary waveform from a Timer. A defined pattern should be generated, after a Trigger from another Timer.The arbitrary pattern works well by DMA, but i cannot trigger it. It's also possible to let it ru...
I am using STM32H503.I want to receive only incoming ids as 0x222 using masking .If set like the code below, IDs other than 0x222 are also entered into the rx callback function. Is there something wrong with the masking process?FDCAN_FilterTypeDef sF...
Dear, FDCAN does not work.Please advise if there is any problem in the entire code below.The set clock of FDCAN is 48Mhz and each setting is as follows.When the code is executed, Tx is transmitted once every 4 seconds in the while loop.However, if Tx...
I'm wondering whether there is a DMA channel to transfer a received message from the CAN fifo to a memory location. Is it possible at all to get DMA working with the CAN controller?Kind regards,Stefan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.