2023-04-13 8:39 AM
NUCLEO-H723ZG
I would like to have a triggered Arbitrary waveform from a Timer.
A defined pattern should be generated, after a Trigger from another Timer.
The arbitrary pattern works well by DMA, but i cannot trigger it.
It's also possible to let it run continously when i disable One Pulse Mode.
But with One Pulse Mode ON, the DMA Update is issued after the next Timer Trigger and not after the last Pulses!
I have DMA Update at TIM_DMA_UPDATE. But TIM_DMA_UPDATE is trigegred when the master Trigger rises. So the DMA is incremented after each Master Trigger.
All samples i found are contiously running..
I dream of a smart Solution with timer settings. Any Ideas/suggestions?
Tnx
2023-04-14 1:41 AM
Try to post concrete information about your setup.
JW
2023-04-14 5:57 AM
Thank you so much so far.
Seem s i need be more detailed.. sorry.
Using CubeIDE 1.12.0 with HAL.
I have TIM4 as Master Timer with TRGO Output UpdateEvent. It produces a fixed cycle (now: 1kHz)
Then i setup TIM1 as Slave: TriggerMode, Trigger Source ITR3, Channel1: PWM CH1, One Pulse Mode
DMA Settings on TIM1: DMA Request: TIM1UP, Circular, HalfWord
Some code:
uint16_t const aSRC_Buffer[] = {5,4,2, 11,4,1, 19,4,14, 50,4,5}; //test pattern
HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1);
HAL_TIM_DMABurst_MultiWriteStart(&htim1, TIM_DMABase_ARR, TIM_DMA_UPDATE, uint32_t*)aSRC_Buffer, TIM_DMABURSTLENGTH_3TRANSFERS, 12);--> The Result is:
Each of this 4 Patterns is sent out. BUT always one single Pattern after the Master Trigger and not one after the other!
-->The Result when switching TIM1 OneShot Mode OFF:
Each of the 4 Patterns is sent one after the other, BUT it doesnt stop when the 4 patterns are sent!
Its continously running.
I can do it by using Interrupts and Start/Stop the Timer:
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim){
if (htim == &htim4 ) {
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
HAL_TIM_PWM_Stop(&htim1, TIM_CHANNEL_1);
}But this is the ugly methot in my view.
Still hope there is a way without interrupts..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.