STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Interrupt not triggered on EXTI1

actually I'm using stm32F446RE, I'm using hal library just to detect external interrupt from PA1 pin but it doesn't work, and if I put the interrupt from PA0 pin, it works fine?/* USER CODE BEGIN 0 */ void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){ c...

kkhli.1 by Associate III
  • 2648 Views
  • 4 replies
  • 0 kudos

Transfer data coming from different devices

Hi ! I am receiving data from two devices and want to transmit it using usb. I am able to send using usb when receiving (to a circular buffer) only from one at a time but when I receive from both, it doesnt work (a lot of data is lost and I cannot d...

LOnGr.1 by Associate III
  • 2330 Views
  • 3 replies
  • 0 kudos

FMAC control loop issue at lower temperatures

Hi,I am currently working on a synchronous buck converter (24 VDC in and 1-15 VDC, 1-15A out) for which I used the HRTIM of the STM32G474 in combination with the FMAC as a control loop:I mainly followed AN5496 and AN5305 to get my converter up and ru...

_legacyfs_online_stmicro_images_0693W00000bjM8UQAU.png _legacyfs_online_stmicro_images_0693W00000bjMAMQA2.png
empps by Associate
  • 1342 Views
  • 0 replies
  • 0 kudos

Flashing Nucleo-L073rz using the system bootloader.

Hello, I have the project in which I need the flash the stm32L0 with uart using the system bootloader. I have settted required option bytes. I make the boot 0 pin high and the sytem is getting into the bootloader mode. I attach the usb to uart conver...

ABans.3 by Associate II
  • 3533 Views
  • 6 replies
  • 0 kudos

Multile definition Error

I am developing my own driver for a STM32 MCU, however I always get the same error when I try to compile the code. Here is the entire code from all the files I developed.There are always 8 errors, saying that pGPIOA, pGPIOB, pGPIOC, pGPIOD, pGPIOE , ...

STM32U5 MCU FFT Performance Testing

I'm using a B-U585I-IOT02A discovery kit that that has the STM32U5 MCU. I'm looking to evaluate if the STM32U5 MCU can run an FFT in real time and how to evaluate the performace of the STM32U5 MCU running FFT's. Are there any tools to help me do that...

PNada.3 by Associate II
  • 12838 Views
  • 1 replies
  • 0 kudos

How to configure GM65 QR Module using UART

I am using L476RG ST board, and I recently purchased a GM95 QR scanner that supports standard TTL-232 serial communication. UART2 is configured to work with my PC using PuTTY as an interface, but how do I receive the data from the QR scanner and disp...

stmmm by Associate II
  • 3584 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H725 reinit MPU.

Hi.Is it possible to reconfigure one or some regions MPU without fully disabling MPU?I need configure for example ITCM memory for RW access when load code and set to RO mode after code copied completed.Code copied from SDRAM to ITCM, so MPU needed fo...

Aleks by Associate III
  • 1461 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.