STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the problem with this display, I am using the STM32F7508-DK With 800x480 Display but I am getting artifacts when using transition function in touchgfx

I am using TST070CBOT-01P Along with STM32F7508-DK using RGB Interface , I have wired the jumpers with the display to the corresponding pins and everything works fine in static mode, But when transition begins then the Display shows artifacts as show...

Caan by Senior
  • 3701 Views
  • 8 replies
  • 0 kudos

Resolved! evaluate both adc on STM32373C-EVAL

I would like to know for this product STM32373C-EVAL if the board has a microcontroller to program so that I can evaluate both adc and read data from both adc. and where do i get the steps from software

anaeb.1 by Associate III
  • 2397 Views
  • 3 replies
  • 0 kudos

CAN2 in STM32F407 is not working

I wanted to us CAN2 interface in my project. I started with example application ("CAN_Networking"). This example application works very well with CAN1 but when CAN2 is configured in this application it doesn't work at all. No transmission and no rece...

Resolved! STM32H743 + QSPI for AD7616

My development environment is stm32cubeMX and IAR.1.Init QSPI2.Read data via QSPIif the DummyCycles = 0,the program is running abnormally.if the DummyCycles over 2,the program is normally.int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ ...

_legacyfs_online_stmicro_images_0693W00000dK0VFQA0.png
wqw.1 by Associate II
  • 2666 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.