2023-06-05 5:08 AM
Hi everybody,
I am currently implementing a LDC3114, which has a burst mode that auto-increments the register address i want to read. The data sheet states:
"For both write and read, the address pointer will auto-increment as long as the controller acknowledges."
It's not clear to me if this is something supported by the HAL function. Can I inhibit the ACK after a certain amount of data?
Best regards, Marcel
2023-06-05 5:29 AM
Using the HAL I2C library you just read the wanted number of bytes in master mode and the controller will properly end the sequence. Use a logic analyzer to confirm.
2023-06-05 5:50 AM
Ah, okay, so I am overthinking this. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.