STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using CAN2 (slave) without CAN1 (master)?

Hi, I have just received a custom PCB using STM32F413RG (64 pin package) for a university design competition. We are using a single CAN bus (CAN2) for this PCB. I was trying to get CAN communication working and I only managed to get some junk data fr...

3pak by Associate II
  • 5590 Views
  • 7 replies
  • 2 kudos

How to receive CAN messages inside Timer interrupt.

I use STM32F105RCT6, Where I need to receive CAN data inside a timer interrupt. Also, the IRQ number of the CAN is lower than that of the timer. CAN message is filled to the FIFO0 but "HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan1)" is n...

SPeri.1 by Associate II
  • 2184 Views
  • 3 replies
  • 0 kudos

SPI write and reading from PN532 using HAL not working

I am working on a project to communicate with PN532 nfc reader.The reader work just fine with arduino code using SPI.Below is the library I used to read and write data from PN532https://github.com/adafruit/Adafruit-PN532Now I switched to stm32 board ...

0693W000005Av1kQAC.png 0693W000005AvEyQAK.png 0693W000005Av2YQAS.jpg
KYou.1 by Associate II
  • 3603 Views
  • 2 replies
  • 0 kudos

Missing I2C STOP condition

RM0394 (STM32L4..) in section 37.7.2 describing I2C_CR2.START bit states:"setting this bit generates a START condition once the bus is free"Section 37.4.8 reads:"the master automatically sends the START condition followed by the slave address as soon...

I2C-STOP.png I2C-NO-STOP.png I2C-STOP-START.png
TDJ by Lead
  • 5477 Views
  • 3 replies
  • 0 kudos

STM32L4 dual regular simultaneous mode using dual DMA as I don't want overrun of data. I want to know correct IOC setting for this mode.

I wanted to know how to configure the ioc setting for dual regular simultaneous mode. I want to use ADC1 and ADC2 together. After the correct ioc setting, how to know to code for this mode. I took help of the available resources but getting an error ...

_legacyfs_online_stmicro_images_0693W00000dJxizQAC.png _legacyfs_online_stmicro_images_0693W00000dJxiuQAC.png _legacyfs_online_stmicro_images_0693W00000dJxipQAC.png
AKhot.1 by Senior
  • 1031 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.