STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC via DMA conversion time on Nucleo-C031C6

Hello, I have an issue with the ADC conversion timing while using the DMA controller.I have only configured 1 ADC channel, 12b res. and the ADC clock is at 24MHz (50% of SYSCLK), and it shows correct conversion results (verified by a simple voltage d...

DDjur.1 by Associate II
  • 3490 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H503RB I3C Target Address NAK Problem

I am using EVB NUCLEO-H503RB with I3C Target feature. I have successfully assign a dynamic address (0x50) to this I3C Target: However, I could not get ACK from this Target with Address 0x50:   Below are my configure, is there anything missing for res...

kh_placeholder.png kh_placeholder.png kh_placeholder.png
BRIAN_LAI by Associate II
  • 3520 Views
  • 3 replies
  • 2 kudos

Can not read register base when enable ICache

Hi,I have an issue reading UID_BASE_ADDRESS. It seems to work fine when the ICache is disabled, but you're unable to access it when the ICache is enabled.Please help me resolve this.Best Regards,

HNguy.27 by Associate II
  • 904 Views
  • 1 replies
  • 0 kudos

CubeMX not generating the correct MX_GPIO_init()

Hello, I am working with cubeMX and trying to configure a pin to output mode. The MX_GPIO_init()  is not generated correctly, there is just clock enabling of the bus connected to the GPIO ports without the configuration of the pins. I am using CubeMX...

ALoua.1 by Associate II
  • 3378 Views
  • 6 replies
  • 0 kudos

STM32H7B0 (A0). Is it possible to copy data from an sdcard to an external qspi rom to be used as program rom (.romdata)?

Is it possible to copy data from an sdcard to an external qspi rom to be used as program rom (.romdata)? I am currently reading data from an sdcard card using fatfs to const program in the. (.data) section but it is a memory hog. Are there any examp...

I have an issue with the HAL_DMA_TransmitReceive() function. I am using full-duplex SPI communication between STM32F030R8T6 as master, and Nucleo-C031C6 as slave. I am only using DMA on the master side. My DMA clock is at 40MHz, SPI clock is at 10MHz.

The problem is I can successfully transmit-receive up to 4 bytes of data. Above that amount, anomalies happen. I need to transfer 20 bytes of data in both directions. Does this have anything to do with RXFIFO and TXFIFO buffers being 4 bytes, or is i...

DDjur.1 by Associate II
  • 2037 Views
  • 4 replies
  • 0 kudos

Can't get ADC values

I have an STM32G474RE, I have not used any HAL or LL libraries, I have only programmed using the registers, my issue is that I am only getting 0 on the output of the ADC, I read through the reference manual and still couldn't solve the problem. I hav...

_legacyfs_online_stmicro_images_0693W00000dDeuQQAS.png
Epsilon03 by Associate II
  • 5965 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.