2023-06-13 12:57 AM
The problem is I can successfully transmit-receive up to 4 bytes of data. Above that amount, anomalies happen. I need to transfer 20 bytes of data in both directions. Does this have anything to do with RXFIFO and TXFIFO buffers being 4 bytes, or is it something else?
Thanks!
2023-06-13 2:05 AM
I guess the problem lies in the slave software but since you are not showing it there is no way to help you. SPI slave in not an easy thing to do on any MCU.
2023-06-13 2:18 AM
Thank you for your time and the response!
Here are some relevant code snippets:
SLAVE code segments for problem description:
#define FRAME_SIZE 4
/* Receive data buffer (MOSI line) */
uint8_t rxData[FRAME_SIZE];
/* Transmit data buffer (MISO line) */
uint8_t txData[FRAME_SIZE];
/* txData buffer fill test */
for (int k = 0; k < FRAME_SIZE; k++)
txData[k] += k;
/* Skipping unimportant lines of code for problem description purposes... */
int main(void)
{
/* Skipping unimportant lines of code for problem description purposes... */
MX_SPI1_Init();
HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t *)&txData, (uint8_t *)&rxData, FRAME_SIZE);
while (1)
{
}
}
void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_HARD_INPUT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t *)&txData, (uint8_t *)&rxData, FRAME_SIZE);
while (SPI1->SR & SPI_SR_BSY) {};
/* Data update test */
for(int k = 0; k < FRAME_SIZE; k++)
txData[k]++;
}
2023-06-13 4:05 AM
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
/* Data update test */
for(int k = 0; k < FRAME_SIZE; k++)
txData[k]++;
HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t *)&txData, (uint8_t *)&rxData, FRAME_SIZE);
}Try the above. Your original code blocks the interrupt and modifies the data while it should be transmitted.
2023-06-13 4:21 AM
Thank you for the reply! That is why I did this 'while (SPI1->SR & SPI_SR_BSY) {};' inside my original code. However, I tried your version and anything above 4 bytes does not cause the slave to ever go into the HAL_SPI_TxRxCpltCallback() function. If you have any suggestion as in why that may happen, it would be of great help.
Thanks a lot! :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.