STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help with Led blinking - STM32F7508-DK

Hi folks, first off all I'd say to that I'm really new to MCU and for some silly reason I went for a STM32F7508-DK as my first board of STM3. With that being said, I'm asking for help on why my Led blinking code is not working,/* USER CODE BEGIN Head...

MCosm.3 by Associate
  • 4033 Views
  • 4 replies
  • 1 kudos

Best use of timer and timer modes

Hello all and tks for reading,I will develop a three-phase 60Hz rectifier, 12 pulses, thyristor controlled. The mpu to be used is the stm32f303RE and I will make the prototype on a Nucleo-64 board.The mpu control signals will go to an already existin...

LCatL by Associate II
  • 3133 Views
  • 2 replies
  • 0 kudos

I am using a STM32G474 and testing it in a nucleo-64 board. When I enable the hardware window watchdog and the hardware independent watchdog my software does not run. it seems to get stuck after each startUp.

The hardware watchdogs is set through an option byte modification done by software and right afterwards the WWDG and IWDG init functions are called as well as the refresh API, called periodically. If I change my code to use the SW WWDG and IWDG then ...

AMija.1 by Associate
  • 1472 Views
  • 1 replies
  • 1 kudos

CAN RX interrupt invokes LTDC error upon exit

This is a weird one :) I'm using the STM32F769 device, and I have the LTDC peripheral running at low speed (8MHz PCLK). When I send a CAN message to the unit, the CAN RX interrupt is invoked, and only when the ISR exits,  an LTDC error interrupt is r...

RShan by Associate II
  • 935 Views
  • 0 replies
  • 0 kudos

HRTIM

which registers should I use to set to set the flag in the HRTIM_TIMxISR register   O1STAT: Output 1 Status Output 1 was active   I think this is a normal question, because I see a discrepancy between the documentation and the behavior of the microc...

MTS by Associate II
  • 3017 Views
  • 3 replies
  • 0 kudos

Resolved! RM0456 - repeating chapters in Bookmarks

In Bookmarks, first 5 chapters are repeated: The same was with 'L4 manuals, lazy to look up the thread, I wonder whether those are fixed [EDIT] found it https://community.st.com/t5/stm32-mcu-products/rm0351-repeating-bookmarks/m-p/120032 [/EDIT]JW

waclawekjan_0-1687867032533.png

Resolved! STM32L100RC temperature sensor

Does the STM32L100RC have a temperature sensor?RM0038 refers to the temperature sensor in the STM32L1 line of processors. However, the STM32L100RC datasheet only mentions "tempsensor" in table 4 and nothing else anywhere. CubeIDE will allow the tempe...

km by Associate
  • 4674 Views
  • 3 replies
  • 1 kudos

PLL Maximum input jitter

What exacly is the maximum acceptable jitter for the input reference clock ?The chip we are using is the STM32U585QIIx. We consider using an external clock from a VCO as HSE, and increase the frequency of the clock using the internal PLL. The VCO is ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.