STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does STM32G050K6 have Unique ID?

There is "96-bit unique ID" in the datasheet (DS13514 Rev 2 ). The feature is also listed on product page . But there is no mention of unique ID in the reference manual (RM0454 Rev 5). Does the MCU have unique ID and how it can be accessed?

STM32L476 (Nucleo64), BLE scanner using BlueNRG-MS stack

Hi everyone,I'm working with a Nucleo-64 evaluation board equipped with an STM32L476. To make BLE I added the IDB05A1 module.I want to create a simple scanner, but browsing through the examples in ST32CubeMX, I can't find an example of a scanner usin...

GBara.3 by Associate II
  • 952 Views
  • 0 replies
  • 0 kudos

Resolved! STM32 custom board with stlink binary

Hi, We want to incorporate the STLink firmware binary provided by STMicroelectronics here onto our custom STM32 board with stlink circuit. However, we would like to seek clarification on whether this usage would allow us to sell our custom board comm...

n.serina by Associate III
  • 3851 Views
  • 5 replies
  • 0 kudos

STM32L151VE ADC

"The ADC of STM32L151VE is not functioning properly. The output values of the ADC appear to be random. Does anyone know how to resolve this issue?

20230627145511809.jpg

STM32F4. Transfert data from SPI3 to SPI1 and DMA ?

Hello,I need with STM32F4 to read datas (multiple bytes) from a sensor connected to SPI3 and transfert the bytes i read from this SPI3 to an external memory connected to SPI1.I would like to use DMA (if possible). Seemingly SPI1 can only be connected...

FMaup.1 by Associate II
  • 1967 Views
  • 2 replies
  • 0 kudos

Resolved! How to measure power supply internally on STM32F107?

Hello community, I'm working on a STM32F107VCT6 where I have practically (by means of very basic filtering) shorted on the PCB VDD/VDDA/VREF+/VBAT and VSS/VSSA/VREF-.   I've runned out of pins so I was wondering if there were a way to measure the pow...

Spaghetto by Associate III
  • 6612 Views
  • 5 replies
  • 3 kudos

Resolved! Help in selecting a dev board

I have over 25 years in embedded design but I am new to ST and ARM cores. I am looking at the STM32 MCU's to replace a 32bit MCU I am already using, the only feature I don't need is the graphics system as we have our own GUI hardware and firmware. I ...

laffelt by Associate
  • 2175 Views
  • 2 replies
  • 0 kudos

Resolved! FLASH ECC Codes Cause Bus Fault on STM32H743

Hello,For a few months now I have been having issues with writing data to flash memory on the STM32H743ZIT6. Most of the time, everything works great and I am able to read the data from flash successfully, but every now and again, the flash memory ge...

0693W00000StskjQAB.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.