STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading RPM from Motor using hall encoder

I am trying to implement a code that can read the velocity of a DC motor with built in encoder. I am using STM32 F446RE and a CQrobot motor equipped with an Hall encoder.. specifications below:http://www.cqrobot.wiki/index.php/DC_Gearmotor_SKU:_CQR37...

totino5 by Associate
  • 5484 Views
  • 0 replies
  • 0 kudos

Resolved! DMA access on M7 Device

I'm using a STM32H745 MCU, with two processors, one of which is an M7. With the M7 I have problems with the DMA, I have seen that it is a very discussed topic on the internet, where there are many solutions, but I still have some doubts: I would like...

FMass.1 by Associate III
  • 1607 Views
  • 1 replies
  • 0 kudos

CANBUS Working on Loopback but not in normal

I am trying to set up a CANBUS connection between two STM32L4 Microcontrollers and while having has been setup correctly and none of the microcontrollers are sending error messages I cannot seem to get a Receive message from either CAN transceiver.Th...

External power supply STM32L432KC

Hello,I was experimenting with the L432KC board. While connected to the computer everything worked fine, but as soon as I tried to use an external power supply everything stopped working. More specifically the board's led LD1 slowly flashes when conn...

Resolved! Fluctuations in ADC value of STM32H743 MCU

Hi,I have been working with STM ADC’s from quite a long time. I had used STM32F373 and F4 series MCU ADC’s earlier for my applications. As, now my application requires huge amount of RAM, memory and computation speed I have shifted to STM32H743 MCU ....

James1 by Associate II
  • 23722 Views
  • 26 replies
  • 3 kudos

DMA - from SPI to DAC - 16 bit

Hi,I use DMA for transfer data from external flash memory to DAC for playing sounds - in 8 bits mode like that:1) TIM6  gives impulses to DMA_1 - which transmit  dummy byte to external flash in 8 khz intervals (Fsampling of sound). External flash alw...

JR2963 by Senior II
  • 1930 Views
  • 2 replies
  • 0 kudos

Multiple pulses are generated on GPO pin for ST25DV64KC micro, when NFC enabled mobile is kept near the antenna, it is expected to have only two pulses for RF activity entry and RF activity exit conditions

Hi,I am using ST25DV64KC micro for NFC communication interfaced with SAML micro controller. I have kept the setting for GPO signal as I should two pulses for every RF read/write session, first one indicating RF field is active and another one indicat...

SSBH by Associate
  • 1246 Views
  • 1 replies
  • 0 kudos

STM32 development board for CAN/OBDII development

Hello. I am looking for STM32 based development board for CAN/OBDII development. Please suggest me some suitable supportive development board based on STM32F4 or H series which has inbuilt CAN support and if it has CAN/OBDII development support examp...

ASh.1 by Associate II
  • 4428 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.