2021-08-23 4:28 AM - last edited on 2023-06-19 7:51 AM by Amel NASRI
I'm working on my project with L432KC which can support only I2C.
I need MCU board which is supporting I3C communication.
Solved! Go to Solution.
2023-06-20 1:51 AM
Hello @TKim.4 ,
If you are looking for MCU which is supporting I3C communication, I suggest you to use STM32H503, STM32H562/STM32H563 or STM32H573.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-08-24 12:57 AM
Hello @TKim.4 and welcome to the Community :)
This feature will for sure be introduce later, but there is no information to share regarding the availability or the supported MCU.
I invite to follow the roadmap in coming months.
Imen
2021-08-24 4:25 AM
Thank you for your answer.
I hope to hear the news soon.
2022-11-13 10:03 PM
Hi @Imen DAHMEN .
Is there a any update on I3C function?
And I'm also looking for MCU board supporting SPMI.
Thank you.
2023-06-20 1:51 AM
Hello @TKim.4 ,
If you are looking for MCU which is supporting I3C communication, I suggest you to use STM32H503, STM32H562/STM32H563 or STM32H573.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-27 1:43 AM
Hi @Foued_KH
Thank you for checking it.
There is one more question.
Is there an STM board that supports SPMI interface?
I'm looking for it through the website, but I don't have any information.
Regards,
2023-06-27 2:35 AM
Hi @TKim.4
Please create a new thread for this question as this one is not about System Power Management Interface (SPMI) but about I3C.
Thank you and best regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.