STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CRC data ignored after CRC reset

[This is a reconstruction of a thread I've started on Apr 7, 2017, but got lost in the two forum software transitions since then.]CRC unit is reset by writing CRC_CR.RESET to 1.If immediately after this data are written into CRC_DR by the processor (...

waclawekjan_0-1691334986006.png

Resolved! How can i use i2c4 on STM32H750B-DK?

I'm testing i2c4 on STM32H750B-DK board with DS3231 but I think that i2c4 peripheral is not worked as i expected.1. CubeMX settings - Only set SYS, RCC(HSE-Crsystal/Ceramic Resonator), USART3(115200 bps), I2C4(PD12: I2C4_SCL, PD13: I2C4_SDA)) after c...

David Kim by Associate II
  • 3594 Views
  • 5 replies
  • 0 kudos

STM32U5 AWS Virtual workshop

Hi,We are working on a project based on the x-cube-aws package. I used the script from the GitHub STM32U5 AWS Virtual workshop to setup the project. The script STM32U5_AWS_VWS_PrereqCheck.ps1 runs successfully. I got the error below when building the...

sliu1314 by Associate
  • 935 Views
  • 0 replies
  • 0 kudos

Custom PCB detection

I designed a PCB using STM32L476RG and MPU6050. I used USB interface in the board. When I am connecting the board to my laptop the board is getting the power but laptop is unable to detect the board. Should I install any drivers in my laptop to make ...

Tracing Source of Double Precision Libs

I'm building an application for an STM32G0 and noticed that quite a bit of double precision libs such as _strtod_l, __aeabi_dsub, __aeabi_dadd, etc are shown in the linker file. As far as I know, there is no double math being done but obviously somet...

Konami_0-1691183156487.png
Konami by Senior II
  • 5872 Views
  • 9 replies
  • 3 kudos

Resolved! STM32G070 ADC DMA - Invalid value in array.

Hi.I am using STM32G070RB.I need to sequentially receive values from 5 channels using ADC DMA.If normal circumstances, the ADC data of PA0 should be stored in Array[0] and the ADC data of PA1 should be stored in Array[1].However, currently experienci...

img1.png img2.png img3.png img4.png
Todg by Associate II
  • 3351 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.