2023-08-03 10:35 PM
Hi,
Im using stm32h7 mcu for my project.Which is an iot product.I need to use low power mode on it i need to wake the mcu using an gpio external interrupt or either by an uart .Device is switch to some mode with a constant current consumption which is a bit higher value.There is only a 20mA difference with run mode on this state.
these are the code which is used to make mcu to low power mode.
ATOMIC_SET_BIT(huart1.Instance->CR3, USART_CR3_WUFIE);
WakeUpEventConfig.WakeUpEvent = UART_WAKEUP_ON_STARTBIT;
HAL_UARTEx_StopModeWakeUpSourceConfig(&huart1, WakeUpEventConfig);
HAL_UARTEx_EnableStopMode(&huart1);
HAL_SuspendTick();
HAL_PWREx_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D1_DOMAIN);
What should be the reason to have higher current consumption in this mode(im getting around 82mA constant in this mode and getting an increment on run mode to 100mA)?
2023-08-04 2:25 AM
Hello @Error_Code,
Could you share the full configuration of your test: SystemClock_Config(), VOS, flash memory status and all the parameters in this table.

Also, there is an example code using stop mode in the STM32H7CubeFW following this path : STM32Cube\Repository\STM32CubeH7-master\Projects\STM32H747I-DISCO\Examples\PWR
Finally, make sure to set all unused pins to analog as shown in this article : How to minimize the power consumption in low power mode: An example using NUCLEO-F401RE board
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.