STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750B-DK ADC Sample

Hello there, I am making an osciloscope I am using ADC with configuration like thisand I am triggering my ADC with 1ms TIM6 and sending this to PC where I display it I am using 240Mhz CPU Clock and my clock configuration looks like this Now everythin...

ADC1.PNG ADC2.PNG Clock1.PNG Clock2.PNG
MKocj.1 by Associate II
  • 5968 Views
  • 7 replies
  • 1 kudos

How to send USB Host 512 bytes long data using STM32U575

Dear All,I am developing an application for USB host mass storage class for STM32U575.I am using STM32HAL APIs for developing USB host and using TinyUSB open-source USB stack.I am able to enumerate flash drive successfully, but not able to perform so...

RRajb2_0-1693568850898.png
RRajb.2 by Associate III
  • 4463 Views
  • 7 replies
  • 0 kudos

STM32H750 to STM32WB

I am looking to add bluetooth onto my project. I have an already developed nRF52 project I could use and just connect it through UART to the STM32H750 or migrate my STM32H750 to a WB based MCU since it has onboard bluetooth connectivity. I was wonder...

MAlan.1 by Associate III
  • 2091 Views
  • 2 replies
  • 2 kudos

Build compiler error

I am using STM32U575ZI cortex- M33 controller. I am able to generate a code for the same micro controller in CUBE MX. But in Cube IDE I couldn't able to build the files. It shows some compiler error. like,"../Drivers/CMSIS/Include/cmsis_gcc.h: In fun...

SivM by Associate II
  • 3714 Views
  • 5 replies
  • 1 kudos

STM32H753 How to test ECC on L1 cache

Hello,I am using a STM32H753. I would like to test the ECC on the L1 cache. In my understanding, a double bit error on the data cache would trigger a BusFault: is there a way to produce it? Thank you

lwen by Associate
  • 1234 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.