STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB VBAT and controller power

Hi , I am using STM32L072CBT6 for my project. We have to use USB for configuration purpose. The controller VDD is connected to 1.8V power supply, but the VDD_USB is 3.3V. Is there any issue to connect 2 different powers ? 

Deepu joy by Associate II
  • 1257 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 RTC maximum current consumption in VBAT mode

With reference to STM32L496xx datasheet (DS11585 rev 17) page 152 table 49, can maximum values be provided for IVDD_VBAT with RTC enabled and clocked by LSE quartz, for VBAT=3.0V and at 25°C and 55°C? (The red marked cells)

S.Nygaard by Associate II
  • 3184 Views
  • 2 replies
  • 0 kudos

hard fault

HiI encountered a strange problem regarding HardFault .The issue occurs when SW is running on STM32G030K8T6BUT DOSNT OCCUR when running on STM32G031K8T6 !!!My SW is basically a power supplyer doing the followingTIM1.4 triggers ADC -> DMA -> IRQTIM1.2...

yona by Associate
  • 2931 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F207VGT6

Hello everyone. I was looking for the schematic of the STM32F207VGT6 but couldn't find it. Can anyone share this if they have it? Thanks. 

haokerem by Associate II
  • 5700 Views
  • 8 replies
  • 0 kudos

Resolved! VREF Wiring stm32l4

After playing around a bit and talking and googling some stuff is my vref wiring correct our should 3.3VA be removed as in some other examples

New Screen Shot Name 2023-09-09 at 20.23.06.png

STM32WB Zigbee to Raspberry Pi Xbee connection

Hi,I'm working on a project where Raspberry Pi together with Xbee s2 (if possible) will work as a coordinator. On the RPI there will be a frontend and node js backend hosted. I want to use xbee module s1 or s2, as I already have a few. For the end de...

DWuje.1 by Associate II
  • 2754 Views
  • 3 replies
  • 0 kudos

Resolved! VREF Pins stm32l496ZGT6

Hello im new to embedded design in general and have a simple question for the vref pins on my stm should i directly wire vref- to ground and vref plus to my 3.3v supply or is there another way this is done:grinning_face:?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.