STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO connection on MCU

Hello,I'm relatively new to PCB designing and I've already learned a lot of things, but I'm still not sure about connecting 2 components through GPIO pins. I have IIS2MDC magnetometer and I would like to connect INT/DRDY pin to STM32H747AI. Let's say...

GPIOs.png MAG.png STM32H7.png

STM32L4 wakes up instantly from low-power sleep

Hi all,I want to measure the power consumption on my board which has a STM32L431CC. Other than the µC, there is nothing left on the board excepted for an RC filter on the NRST pin, I removed the RTC quartz.Inspired by the example code i found, i wrot...

Steven.D by Associate II
  • 3123 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO read/write not working on custom STM32H735 board

Hello,I'm using a custom board based on a STM32H735 with various GPIO inputs and outputs. The STM32 is packaged as a 0.5mil pitch BGA and the board assembly has been outsourced.I'm able to flash a program on the MCU and debug it by adding breakpoints...

Using timer to wake from sleep

Im attempting to put the cpu to sleep between ticks of timer 15 on a stm32L432, The LED flashs without the Sleep code however it never wakes up from the timer interuptvoid HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef * htim) { HAL_ResumeTick(); if...

PGood.1 by Associate II
  • 4883 Views
  • 2 replies
  • 0 kudos

Resolved! Confusion with MDF and its SPI/Manchester setting

Hi all,We are trying to wire a microphone to the STM32U585. The microphone (T5838) outputs PDM and takes a clock as input.As far as I understand, the MDF peripheral supports PDM interface (as stated in RM046, Rev 4, 39.1), so it is compatible with th...

VTOR_S when TrustZone is disabled

Using the latest STM32CubeIDE, STM32CubeH5 and NUCLEO-H563ZI with TrustZone disabled.I put a breakpoint at the first instruction in startup in Reset_Handler. The debugger shows in SFRs, SCB->VTOR_S is 0x8000000 (which is my NSBOOTADD) and SCB->VTOR_N...

mete by Senior II
  • 1497 Views
  • 0 replies
  • 0 kudos

STM USART bootloader issue with STM32F446

I've been using bootloader over USART3 PB10/PB11 at an STM32F446ZET6 for long time and it works reliably at least at 115200kbit.  This year we assembled several new PCB's without HW change and the bootloader stopped working. When programming the STM3...

MartenP by Associate
  • 3524 Views
  • 3 replies
  • 1 kudos

Resolved! Write Flash memory over virtual Com Port (USB)

Hello, I am developing a dual processor application with a host (STM32F205xx) and a slave (Radio Module SoC). The idea is to update the wireless module's firmware from the PC via the virtual COM port.The firmware is temporarily stored in STM flash me...

Semiory_0-1694441426331.png
Semiory by Associate II
  • 2585 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F411 Discovery board Blink LED program error simulink

I am trying to run the Getting started with stm32f4discovery project in matlab simulink. the code simple wont run. I tried multiple methods and answers however my error is always related to USB connection issues.  "Error while trying to establish USB...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.