Resolved! "UM2407 Rev 3 User manual", table 18, "CN7 ZIO Connector pinout" pin name of pin 14 wrong
Hi,while doing a symbol for the Nucleo in KiCad I found that the Pin CN7.14 should be PA7 instead PB5.The sub-note (3) is correct.Best regardsMarco
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi,while doing a symbol for the Nucleo in KiCad I found that the Pin CN7.14 should be PA7 instead PB5.The sub-note (3) is correct.Best regardsMarco
Hi,We have used STM32F427IIH6 MCU to create custom board. We assembled first proto batch of 10 boards. All boards were perfectly flashing. While testing one board stopped flashing.Based on error message we checked write protection option byte status....
Hi everyone!In my program I have an input which is turning on and off. If the input is not turn on in 3 second I need to detect this. I'm using Timer14 with interrupt. If the input is turn on, the timer is stopped, reseted and start counting from th...
I have to deploy an algorithm with a lightweight deep learning-based approach on a low-power STM System-on-Chip based on an Arm Cortex-M-class MCU or Arm Cortex-A-class MPU. Is there a way to reduce cache-misses or a way to reduce the CPU stalls on c...
I have been following mastering stm32 book for a while now and checking out the tutorials from the st channel.I was following the dac tutorial and I had a problem with outputting analog signals in pin A4.I use eclipse IDE and i am imporing cube-mx fi...
I'm following the example the USB MSC Standalone example provided here:https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Projects/STM32446E_EVAL/Applications/USB_Device/MSC_Standalone/Src/usbd_storage.cI am attempting to get the eMMC that...
Hi everyone i am new to using peripherals like HDMI and USB with my applications and i wanted to get started with it but i didnt simply want to go with HAL libraries instead i want to understand the basics of them and how to start from scratch. Also ...
Hello, I am facing an issue when trying to calibrate the STM32U5. I am using the API call `HAL_ADCEx_Calibration_Start()`, SDK Version: 1.3.0.When I run the `HAL_ADCEx_Calibration_Start()` the board hangs and goes off into a limbo state. Even the deb...
I am trying to create a repeating trigger to start an SPI transfer to read 12 x 16 bit values from an external ADC.I have configured the SPI with a Rx DMA to receive the data and have created a timer to trigger a second DMA to write to the SPI->CR1 r...
I have a STM32F405 with a coin cell on VBAT and I haven't been able to get the Backup SRAM or RTC to preserve contents when removing main power. The same code works fine on another board that has a STM32F407. //Works on STM32F407 - Fails on STM32F40...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.