STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Incomplet SystemInit() for STM32G474

Hello,Recently I spent some time solving the problem of incorrect CPU operation. After generating the project (completely basic, only TIM6 set as TimeSource for HAL), the program diverged when trying to enter the interrupt from TIM6 (I'm guessing). K...

p2399 by Associate II
  • 2064 Views
  • 3 replies
  • 0 kudos

Which bootloader for STM32F407VET6 ?

Hi,Does anyone know which bootloader to use for this damn board (STM32F407VEt6). I have tested several of them but it is still not recognized by Win10Thank you in advance

FDeri by Associate II
  • 5182 Views
  • 5 replies
  • 2 kudos

Resolved! STM32f302 Operational amplifier 2 reference voltage

Hello Community, I am currently working with a stm32f302rc microcontroller, I need to configure my ADC2 to measure the reference voltage of operating amplifier 2 (Vrefopamp2) (it is internally connected to channel 17 of the ADC).I need this to check ...

Saddrone_0-1695376508950.png
Saddrone by Associate
  • 2167 Views
  • 2 replies
  • 0 kudos

Resolved! 1.8V VDD and 3.3V VUSB

Some STM32's have VDD and VDDUSB. Setting VDD to 1.8V and VDDUSB to 3.3V, the GPIOs work at 1.8 V, and USB keeps working (the USB transceiver needs 3.3V). Each time, there is a note that VDDUSB has to be the last power supply to be active when poweri...

koendv by Associate III
  • 8804 Views
  • 4 replies
  • 1 kudos

Multiple UART implementation

We are using a the Microcontroller for one of our products , we are using two UARTS for communication , however when both the UARTS are enabled we are facing some difficulties in the communication, can anybody help in this ?Attached is the main file ...

Pooshan by Associate
  • 8599 Views
  • 7 replies
  • 1 kudos

STM32U585 SmartCard Mode Init Error

Hi TeamI am working on the ST provided package with TF-M Example and working on adding the smart card interface at uart3(without using cube mx setup). I have a working code with smart code with TF-M Structure(GTZC enabled) and using Cube MX. I used t...

PJose.4 by Senior
  • 897 Views
  • 0 replies
  • 0 kudos

STM32L151 fails to boot with CubeIDE autogenerated code

Hi everyone,I recently triggered a bug in multiple projects using the same MCU STM32L151ZC. When booting the CPU I reproducibly get an assert_failed() call from HAL_RCC_OscConfig(). I created a clean project in CubeIDE to analyse the problem, which I...

D. Reiher by Associate II
  • 2197 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.