STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103CBU6 HAL_Init Hangsup or STM32CubeIDE?

Hello,I am not really new, but i have a courious problem.I have a STM32F103CBU6 device (new), and started a new C++ Project with STM32CubeIDE 1.13.2 and the STM32Cube FW_F1 V1.8.5 firmware package.I have a external crystal for both (HSE + LSE) and is...

Screenshot 2023-10-27 082114.png
Sany by Associate III
  • 4434 Views
  • 2 replies
  • 0 kudos

STM32U575 Reference not working?

I'm using an STM32U575 chip with a couple of it's peripherals. I'm trying to get the ADC1 working. It's currently sampling a few pins, but when I read the data, it seems to always be 4095 (max value). Looking into it further, the VREF+ pin is sitting...

sethkaz by Associate III
  • 3090 Views
  • 6 replies
  • 0 kudos

STM32H743 POWER without LDO

I have designed a board based on STM32H743VGT6. This package doesn't have LDO PIN. Which item in CUBEMX i have to choose for power supply? Do I have to connect voltage to VCAP pins?

Mozh by Associate
  • 2143 Views
  • 2 replies
  • 1 kudos

Web UI on STM32

HeyI want to make a product with WEB UI . My goal is product that will connect to my internal network and I want to be able open a browser on my computer and write the IP of the product, I will connect to its web page and I can control it.I would app...

TOsso.1 by Associate III
  • 7030 Views
  • 4 replies
  • 1 kudos

Resolved! Why is my ADC only showing zero as an output while simulating the stm32f103C6 model in proteus?

The above is my schematic layout of ,STM32F103C6 Series, attached to a virtual terminal with transmitting and receiving lines mentioned and the pin PA2 is used as an ADC input pin.The above is the power rails configuration .The above is the pinout vi...

Krishnangshu_0-1696934804825.png Krishnangshu_1-1696935020724.png Krishnangshu_2-1696935105658.png Krishnangshu_3-1696935358908.png

STM32L452CC SPI send wrong data

Hi, Its my first post. Im trying a STM32L452 and IIS3dwb on SPI2 (SPI2_CLK on PB13). When I send the WHO_AM_I command, the SPI2_MOSI send only 0x0F instead 0x8F (0x0F OR 0x80). SPI2 setup is CPOL = High, CPHA = 2 Egde, 8 bits, MSB First, Baud Rate = ...

dso_01_01_02_11_25.bmp
fmaesso by Associate II
  • 1925 Views
  • 3 replies
  • 0 kudos

How to keep HSI running in STOP mode?

Hello support team.I'm using the STM32L011D4P, I configured the MCO output to repeat the HSI oscillator output divided by 16 and have a 1 MHz signal. With the help of an oscilloscope it is possible to identify a 1 MHz square wave.In the datasheet, I ...

Takahashi by Associate II
  • 3786 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.