2023-10-29 8:41 PM
Hi i have a generic doubt about falsh wait states:
Say we configured the PLL to run system core clock at 160 M Hz, with flash wait states as 5.
Then is cpu is equvilent to 32 MHZ core performance? (assuming 1 clk/ 1 inst, no ART's)
Could some one help me on this so that i will make my understandings better which helps me to choose the right controller for right application?.
2023-10-29 9:45 PM
It means the flash accesses at around 27 MHz (35 ns), but it's not accessing bytes, but rather 128 / 256-bit flash lines, thus one read can sustain multiple MCU instructions.
The H7 also has a cache so that hides latency of slower memories.
2023-10-29 11:00 PM
@Tesla DeLorean thanks for your reply.
By considering 32 bit instruction and const data access (worst case) with 128 / 256-bit flash lines, it could fetch 4 / 8 instructions/data @ 27 M Hz. So apparently the processor speed is (worst) is 54 M Hz (considered 1 isntruction + 2 const data + 1etc)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.