STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

application note and data sheets

In the installed STM32Cube Repository there are hundreds of application notes and data sheets, does anybody know where there is a list of contents?  It would take a long time to open them all to check or get the right grep phrase to search.

billium by Associate
  • 5612 Views
  • 2 replies
  • 0 kudos

Resolved! L431 debug stops after enabling timer update interrupt

Hi all, I have encountered a problem where the debug would stop working as soon as the program hits the line where TIM15's update interrupt is enabled. From there the program appears to be still running but would not stop at any breakpoints and live ...

ZJing by Associate III
  • 4789 Views
  • 8 replies
  • 1 kudos

USB HID sample code

Hi team,              I am using one usb-nfc dongle from microE, to integrate it with my board. That dongle is already has code of HID and it is stand alone is working fine (when I connected it to my laptop directly), however am facing challenges whe...

Shikamaru by Associate III
  • 1447 Views
  • 0 replies
  • 0 kudos

STM32U575VIT6Q I2C interface with LIS2HH12TR is not stable

Hi ST Team,We are using an MCU “STM32U575VIT6Q” and we have connected an ST accelerometer (LIS2HH12TR) to the MCU via an I2C interface. Our schematic design (accelerometer) section is attached. Out of 5 boards we built, accelerometer I2C interface is...

Resolved! USB DFU configuration / use

Hi,I used a F105RCT6 in a custom board, i want to use the DFU mod.When I generate the project with cubemx I select USB DEVICE and DFU mid, i change the clock configuration corectly. I generate the FW, and i flash him.The DFU is running, i open cubepr...

Resolved! tolerance for the decoupling

I'm working on hardware design and have some doubts regarding selecting the tolerance value for the decoupling capacitor for stm32l4 series I have read the application note and data sheet I could not find the value for tolerance.so how can I find the...

vasikarans_0-1698914895304.png

sending same data over DMA

I'm using stm32u535 and LIS3DHTR accelerometer. The accelerometer has a 32 FIFO buffer, and I set it up so that it sends a signal to interrupt pin when FIFO is full. To read data, I need to send 0xE900,0x0000,0x0000 (saved in uint16_t  ACC_READ_ALL_D...

btd5 by Associate II
  • 1353 Views
  • 0 replies
  • 0 kudos

Resolved! Hardfault while using TrustZone STM32H573i-DK

Hi everyone,I'm currently experimenting with a STM32H573i-DK and TrustZone and facing some issues.First I tried enabling TrustZone in the Project Creation Process. When i try to run this empty project using the steps:SpoilerSelect and build the xxxxx...

funkii by Associate III
  • 2132 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.