STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is the cause of erratum "2.10.6 Wrong ADC result if conversion done late after calibration or previous conversion"?

I have a mature project utilizing the STM32L4R5xxx series. The main function uses uC's ADC over about 15 channels. As a rule, the ADC readings are taken at a slow rate -- some triggered every 100 ms, others triggered every 5 seconds, and other trigge...

DDrin.1 by Associate II
  • 5286 Views
  • 7 replies
  • 1 kudos

Flexible SPI clock frequency

Hi,We have a need for arbitrary SPI clock frequencies. I looked at ~10 families and most STM32 micro-controllers seem to be limited to prescalers that divide the PCLK by a power of two. I found the STM32H7 but it is wildly over-specified for our appl...

pietrow by Associate
  • 1777 Views
  • 0 replies
  • 0 kudos

Wakeup from sleep or shutdown via TSC

Hello dear community. I am working on a project with a STM32L462CEU6 powered by battery. In this project we are also using TSC. Now I want STM32 to go in sleep or shutdown mode and wakeup when a touch pad has been touched. So the goal is that TSC mea...

Resolved! HRTIM 100% duty cycle

Hello,is there a solution to generate duty cycles between 0...100% with the HRTIM? I tried up-counting mode and center-aligned mode, but I wasn't able to achieve it. RegardsDominik Schmid

DSchm.3 by Associate II
  • 2410 Views
  • 1 replies
  • 0 kudos

Questions about how some HAL protocoles works in RTC

Hello ! I've been practicing how RTC works in STM32 Nucleo and I've used a code from this website tutorials.   void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc) { z ++; RTC_AlarmTypeDef sAlarm; HAL_RTC_GetTime(hrtc, &RTC_TimeStruct, FORM...

Xenon02 by Senior
  • 2354 Views
  • 5 replies
  • 2 kudos

HSE "overclocking" ?

Heyho,anybody ever put more than 50 MHz from an active oscillator to an F767 / H723 / H735 HSE input?I need a VCO there, and I have a few with 51.2 MHz, so less than +5% over.I'm pretty sure it won't damage anything, but before I start (de-) solderin...

LCE by Principal II
  • 3036 Views
  • 6 replies
  • 0 kudos

Sigfox Provisioning webpage down

Sorry, not sure where to post this.The Sigfox provisioning tool at https://my.st.com/sfxp is down.When entering a valid certificate, the downloaded zip contains only the content "Service unavailable, please try again later".Cheers,Tim Lamborn

Resolved! Dynamic memory allocation in PSRAM

Hi,Currently I am using STM32L4R9 discovery board, which has 16-Mbit (2MB) PSRAM. I have been able to allocate static memory inside PSRAM by using following code and also by changing linker script file (.ld). I have attached my edited linker script w...

SSG by Associate II
  • 5499 Views
  • 6 replies
  • 0 kudos

Issue while using USART as UART

In our application, STM32 micro controller  USART protocol is used as UART full duplex mode. what will be the  conditions to use USART as UART full duplex mode?Already I have disabled CLKEN bit in USART_CR2 register. Though, disabling CLKEN bit in US...

Sruthi1 by Associate
  • 1868 Views
  • 2 replies
  • 0 kudos

Input: Read RC signal to Ouput: ON/OFF led

Hi, I read input PWM signal from RC radiolink (done): duty_cycle range 675-1347And now I want to convert this signal to analog to ON/OFF led, I used MAP funtions and I don't know how to move read_RC to ON led, something's like analogWrite (read_RC, L...

ManhPham by Associate III
  • 1001 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.