STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32f103 Eprom emulation

Hi amazing community.I am working with the following mcu STm32F103Since in the design of our board we didn't insert any real eeprom for saving some data we decided to use a emulation tecnique   provided from ST Here below it is reported the header fi...

SGasp.1 by Senior
  • 6081 Views
  • 9 replies
  • 4 kudos

STM32H747L-Disco with COM35H3P70ULC Display

Hi, i try to get the COM35H3P70ULC Display to work with the STM32H747L-Disco Board using a custom Adapter PCB. The Display is connected using 2 Lane DSI and i tried to configure the DSI Host to communicate with it. I cant get it work or respond to an...

LRees by Associate
  • 1188 Views
  • 0 replies
  • 0 kudos

Dividing Timer

I need advice on setting up a 'primary timer/clock' to toggle a an output pin for 20ms, at a user set frequency of anywhere from 16Millihertz to 16.65Hz ( approx ) with 16 bit resolution. ( user sets value from 0 to 10000 )The primary timer/clock mus...

LMorr.3 by Senior II
  • 2690 Views
  • 4 replies
  • 0 kudos

STM32H745 - Encoder Mode Not Counting

I am trying to interface the STM32H747 with a quadrature encoder-equipped motor to track linear movement. When moving forward, I expect the counter to increment. When moving backwards, I expect the counter to decrement. To do this, I have configured ...

LZ_FS by Associate
  • 1857 Views
  • 0 replies
  • 0 kudos

Resolved! Crypto library rsa signature not matching with openssl

Hi,I would use the STM32 Crypto Library. I have the 4.0.1 version.I just compiled and run the RSA\PKCS1v1.5_SignVerify example on my L4 micro and it is successful. Then, I generated with openssl a new 1024 key pair and signed a custom message. Then I...

lukin by Associate III
  • 2882 Views
  • 5 replies
  • 1 kudos

Resolved! CRC check for received data through UART

Hi,I am sending/receiving data using UART between STM32G4 board and other board. While I am sending the data I am adding the CRC and transmitting it through UART to other board. While receiving how do I check the CRC correct or not.For Eg: From other...

Resolved! STM32H735VGH as VBUS powered device

I'm configuring STM32H735VGH MCU  for communicating by USB_OTG full speed, Device mode and want to power it by VBUS.Suggest me best whether power distribution switch is required or not ?

shaktipg by Associate II
  • 1319 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.