2023-10-19 9:59 AM
Hi everyone,
I'm currently experimenting with a STM32H573i-DK and TrustZone and facing some issues.
First I tried enabling TrustZone in the Project Creation Process. When i try to run this empty project using the steps:
the execution lands in the HardFault_Handler after the call to NonSecure_Init().
Almost the same happens if I try to run the GTZC_MPCWM_IllegalAccess_TrustZone example.
After the call to SECURE_SAU_MPCWM_SetInitConfig(), the execution lands in the HardFault_Handler().
I'm following the steps at the bottom of the Readme file.
Am I missing something or has anyone got an explanation for this behaviour?
I would appreciate any help or resources on this topic.
Best
funkii
Solved! Go to Solution.
2023-11-02 3:57 AM
I just forgot to set the Option Bytes as described in here ...
User Option Bytes configuration:
Please note the internal Flash is fully secure by default in TZEN=0xB4 and User Option Bytes SECWM1_PSTRT/SECWM1_PEND and SECWM2_PSTRT/SECWM2_PEND should be set according to the application configuration. Here the proper User Option Bytes setup in line with the project linker/scatter file is as follows: - TZEN=0xB4 - SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure - SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 meaning no page of Bank2 set as secure, hence Bank2 non-secure
2023-11-02 3:57 AM
I just forgot to set the Option Bytes as described in here ...
User Option Bytes configuration:
Please note the internal Flash is fully secure by default in TZEN=0xB4 and User Option Bytes SECWM1_PSTRT/SECWM1_PEND and SECWM2_PSTRT/SECWM2_PEND should be set according to the application configuration. Here the proper User Option Bytes setup in line with the project linker/scatter file is as follows: - TZEN=0xB4 - SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure - SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 meaning no page of Bank2 set as secure, hence Bank2 non-secure
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.