2023-11-02 1:25 AM - edited 2023-11-02 1:29 AM
Hi, Sir:
Currently using H563ZI (MB1404C) to develop programs.
When VDD=3.3V, MCU works normally
When VDD=1.8V, the MCU functions abnormally (USB function fail), but the specification indicates that it can support VDD=1.8V. Where should I set this on the EVK?
2023-11-02 2:31 AM
Hello @Charles63,
what is the voltage on VDDUSB? Is it same as VDD? If yes, and you are using USB, it must be above 3.0V.
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-02 3:20 AM
hi, Sir
2023-11-07 4:14 AM
Hi, Sir :
How to solve this problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.