STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F767 QSPI Slave

Hi, I have the following questions about QSPI in STM32F767:1.  Is it possible to configure the board as QSPI Slave? I could not find any option in the CubeMX Tool to choose between master and slave. 2. Is the QSPI peripheral of this board strictly li...

SPI Receive

Hi, I am working on SPI to communicate with the AD9959 from analog device, I'm analyzing the MOSI and MISO signal with probes on an oscilloscope and can see that  I can successfully write and read from the device, the thing is that HAL_SPI_Receive() ...

Vueko by Associate III
  • 5743 Views
  • 5 replies
  • 0 kudos

Setting the F407 FSMC WaitSignalPolarity default value

Hi All,I have a 407 connected to an FPGA using the FSMC interface.When I compile my device configuration from ST Cube, the WaitSignalPolarity value in the MX_FSMC_Init routine is always set to: FSMC_WAIT_SIGNAL_POLARITY_LOW. On my system I need this ...

Toneski by Associate III
  • 7556 Views
  • 12 replies
  • 0 kudos

Resolved! Can only transmit one SPI byte?

Hello,I am trying to use SPI1 on the STM32H742VITx.I believe I have configured SPI1 I/Os and CR/CFGR fields correctly.  However, when I try to transmit bytes via SPI I am able to transmit one byte, but after that the SPI_SR_TXC bit remains at 0.  Her...

briankaz by Associate III
  • 4072 Views
  • 5 replies
  • 0 kudos

To write I2C functions using interrupts and DMA

Bonjour, Pouvez-vous me dire pourquoi cette façon d'écrire lors d'une transmission I2c par interruption ou DMA ne fonctionne pas :EN: Hello, Can you tell me why this way of writing during an I2c transmission by interrupt or DMA does not work? annul...

Rom by Associate
  • 1968 Views
  • 2 replies
  • 0 kudos

Resolved! FreeRTOS with a non FreeRTOS app

This question is not very specific. It is quite open ended and is probably best posed to those at FreeRTOS support but I will ask here first as your support is excellent.Having spent months developing a Project that is optimized to the best of my abi...

Resolved! Coding Error

This is a portion of my product code, but i got some problem. When an external interrupt occurs i want to start a timer and increment one variable and when timer reaches 30 seconds i want to display the variable via UART. I will provide my code.when ...

2 ADC channels assigned to 1 MCU pin

I have designed a buck converter that uses the MCU to regulate its output voltage.I am using one pin for the voltage feedback that will be used to regulate the output.  However, because it has to read this pin very quickly, the sample period has been...

SDMMC_FLAG_SDIOIT flag not set - SDIO DMA on STMH7B0

I have adhered to the an5200-getting-started-with-stm32h7-series-sdmmc-host-controller-stmicroelectronics.pdf document and have had a good deal of success implementing CMD53 and CMD52 comms with a slave device but there seems to be a problemThe slave...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.