STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM33 SPI issue

I'm using an STPM33 digital signal processor driven by SPI using an STM32G071KBUX microcontroller. Comunication apparently seems to be ok but if I try to enable the only UART/SPI read error interrupt (into US_REG3 register) using the INT1 and INT2 as...

RCase by Associate II
  • 1061 Views
  • 0 replies
  • 0 kudos

Resolved! vref voltage of stm32f429 disc1

Hello all. I am working with internal ADC can I know what is the internal reference voltage and how to change the internal reference voltage? 

harry123 by Senior II
  • 3029 Views
  • 4 replies
  • 3 kudos

Resolved! SPI mode and UHS-II mode not supported for STM32U5xx

Hello,I have  a very basic question. In the spec of the U5 series there is this: Does that really mean that the U5 would not support talking to an SD card in SPI mode? I find it hard to believe since SPI seems to be the most basic way to interface wi...

broilmont_0-1701362559552.png
broilmont by Associate II
  • 2783 Views
  • 4 replies
  • 1 kudos

Migrating from L431CCU6 to F412CEU6

Hello,I'm planning to migrate from L431CCU6 to F412CEU6 MCU and as per CubeMX, all the pins and power scheme matches. But I see there is Vcap on pin 22 of F412 MCU. Is it okay to skip it with below setup? Adding this cap will need redesign and we wan...

Mallikarjun_0-1701408334254.png

UART TIME OUT

Hello everyone I am trying to receive file form UART through Xmodem protocol I am getting file in debug mode but unable to get into run mode it showing  UART Rx busy basically hanging over these function while (!(HAL_UART_GetState(&huart4) == HAL_UAR...

PESHWA by Associate II
  • 2762 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H750 FMC + LCD

I’m having some trouble related to using the FMC to interface with a LCD. We are using NE1 as chip select, LCD register select is A0, 16 bits of data.  When I’m scoping the signals, I’m seeing the A0 go high during 16 bit writes to 0x60000000 (comman...

SMoon.2 by Associate III
  • 8256 Views
  • 5 replies
  • 0 kudos

Resolved! AES v SAES

Hello,The STM32U585 Reference Manual say these chips have one AES and one SAES peripheral. In turn each of these have an "AES core algorithm (AEA)" component. I expect that to mean that there are two physically independent AEA's on the chip. Is that ...

EC.3 by Associate III
  • 2131 Views
  • 1 replies
  • 0 kudos

Resolved! How to recover continuous data with DMA ?

Hello,I have a program that works in DMA but I would like to put a function to know when the transfer in the DMA is finished so that I can recover the data continuously. Do you have any information on this ? Here is part of my code  HAL_SAI_Register...

DYann.1 by Senior II
  • 6947 Views
  • 11 replies
  • 3 kudos

STM32 DFU protocol DFU_UPLOAD problem

Hello,I am trying to implement the DFU protocol in an Android app. I am following AN3156.I am using UsbDeviceConnection class for the control transfer in android. I am able to write to the memory to any address using the routines described in AN3156 ...

LLope.31 by Associate III
  • 6750 Views
  • 7 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.