STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash erase blocking GPIO updates

I am testing doing flash erase while running code from internal SRAM on a STM32F072B Discovery Board. Having initializing everything with code running in flash, I call a function where itself and all its dependencies exist in RAM. I've verified this ...

link87 by Associate II
  • 15550 Views
  • 11 replies
  • 6 kudos

Receving a string from terminal via UART

Hey, I would like to a string from terminal via UART in order to complete a challange given by Digi-Key YouTube channel in FreeRTOS tutorial playlist. Anyway, I want to take the whole string given by user in terminal, but I couldn't so far. I tried  ...

Resolved! Cannot read ID from external flash (OSPI1) on STM32H735-DK

Hello all, I was trying to follow the example in MOOC - STM32H72x/3x hands-on workshop - 6 Code execution from external FLASHI have configured the OSPI as per the board requirements in CubeMX. But the `OSPI_Init()` function fails while trying to read...

NRedd.2 by Senior
  • 3977 Views
  • 4 replies
  • 0 kudos

Resolved! Can not set up PWM for a different Pin than PA5

Hey,after trying to setup a different PIN for example: PC0 for PWM I just can not get it to work.But this sample code works only for PA5:  #include "stm32f3xx.h" int main(void) { RCC->AHBENR |= RCC_AHBENR_GPIOAEN; RCC->APB1ENR |= RCC_APB1ENR_TIM2E...

SDIO 4 bit mode with STM32CubeMX

I would like to use SDIO with 4 bit mode with FatFS. I use STM32F429I Discovery board and I wired a micro SD card board to it. The SD card is a 16 GB SanDisk Ultra A1 card formatted to FAT32.This is the micro SD card board: https://image.dhgate.com/0...

djhtml by Associate II
  • 25105 Views
  • 28 replies
  • 2 kudos

STM32WB Fast Programming with FSTPG

Greetings,We are adding an OTA procedure to our firmware that depends on a small loader at the start of flash which is responsible for programming the main application written to program flash at a higher address.  The procedure works fine as it is, ...

Could not receive an send Ethernet message at the same time

When using F429 to complish the function of Ethernet, a confused phenomenon appears,message sending and message receiving at the same time, the received message could not trigger receiving interrupt,seems lost. Sending message 462 and receiving messa...

Polumfan_1-1701482193274.png
Polumfan by Associate II
  • 1066 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G030 SPI master read issue

I use in my project stm32g030f6p6 to communicate with ADXL345 by 4-wire SPI. I have no problem with transmition, yet with reading I run into serious problem, that doesn't mentioned in Errata.My SPI configuraton is CPOL 1, CPHA 1, speed 1MHz. I use Lo...

KhPaul by Associate III
  • 8410 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.