2023-12-02 6:58 AM
Hello all,
I was trying to follow the example in MOOC - STM32H72x/3x hands-on workshop - 6 Code execution from external FLASH
I have configured the OSPI as per the board requirements in CubeMX. But the `OSPI_Init()` function fails while trying to read the device ID.
When I comment out the code, I am able to jump to an external application that is loaded by the CubeProgrammer.
I am not sure what is going wrong here. Can somebody help?
I have attached the project as a 7Z file.
OSPI_Init();
OSPI_MemoryMap();
printf("Device will jump to: %X\r\n", IMAGE_DEFAULT_ADD);
if ((((*(__IO uint32_t *) IMAGE_DEFAULT_ADD) & 0x2FFC0000) >= 0x20000000) && (((*(__IO uint32_t *) IMAGE_DEFAULT_ADD) & 0x2FFC0000) <= 0x2FFC0000))
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t *) (IMAGE_DEFAULT_ADD + 4);/*address +4 is an reset vector*/
JumpToApplication = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t *) IMAGE_DEFAULT_ADD);
JumpToApplication();
}
The main looks similar to the one in the MOOC video.
I believe that the GPIO configuration is correct because I am able to jump to the external application located at OSP1_BASE.
Solved! Go to Solution.
2023-12-02 9:22 AM
Ok, so what's the error reported?
uint32_t OSPI_Init()
{
uint8_t id[20];
OSPI_RegularCmdTypeDef sCommand;
hospi1.Instance = OCTOSPI1;
HAL_OSPI_DeInit(&hospi1);
hospi1.Init.FifoThreshold = 32;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MACRONIX;
hospi1.Init.DeviceSize = 26;
hospi1.Init.ChipSelectHighTime = 2;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 0x3;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = 0;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
OSPI_ResetMemory();/*reset OSPI memory*/
/* read ospi memory ID */
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytes = 0x00;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesSize = HAL_OSPI_ALTERNATE_BYTES_8_BITS;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.Instruction = READ_ID_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_NONE;
sCommand.NbData = 20;
sCommand.DataMode = OSPIDataMode;
/*send cmd to read ID*/
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/*receive the ID*/
// if (HAL_OSPI_Receive(&hospi1, id, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
// {
// Error_Handler();
// }
OSPI_OctalStrModeCfg(&hospi1);/*set OSPI mode to 8bit DTR*/
return 0;
}Make sure the data mode is correct
...
sCommand.NbData = 3; // Only reports 3
sCommand.DataMode = HAL_OSPI_DATA_1_LINE; // Use SPI mode
/*send cmd to read ID*/
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/*receive the ID*/
if (HAL_OSPI_Receive(&hospi1, id, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
2023-12-02 7:57 AM
You can't send commands in Memory Mapped mode, so either don't do that, or send a HAL_OSPI_Abort() to stop it.
2023-12-02 8:51 AM
The command to read ID is sent before the memory mapping is enabled. It is called within the OSPI_Init(); function.
The command is sent in SPI non-DTR mode.
2023-12-02 9:22 AM
Ok, so what's the error reported?
uint32_t OSPI_Init()
{
uint8_t id[20];
OSPI_RegularCmdTypeDef sCommand;
hospi1.Instance = OCTOSPI1;
HAL_OSPI_DeInit(&hospi1);
hospi1.Init.FifoThreshold = 32;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MACRONIX;
hospi1.Init.DeviceSize = 26;
hospi1.Init.ChipSelectHighTime = 2;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 0x3;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = 0;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
OSPI_ResetMemory();/*reset OSPI memory*/
/* read ospi memory ID */
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytes = 0x00;
sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesSize = HAL_OSPI_ALTERNATE_BYTES_8_BITS;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.Instruction = READ_ID_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_NONE;
sCommand.NbData = 20;
sCommand.DataMode = OSPIDataMode;
/*send cmd to read ID*/
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/*receive the ID*/
// if (HAL_OSPI_Receive(&hospi1, id, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
// {
// Error_Handler();
// }
OSPI_OctalStrModeCfg(&hospi1);/*set OSPI mode to 8bit DTR*/
return 0;
}Make sure the data mode is correct
...
sCommand.NbData = 3; // Only reports 3
sCommand.DataMode = HAL_OSPI_DATA_1_LINE; // Use SPI mode
/*send cmd to read ID*/
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/*receive the ID*/
if (HAL_OSPI_Receive(&hospi1, id, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
2023-12-02 9:25 AM
Thank you for the solution, it works now with the changes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.