STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC SRAM read data sampling time

Hi,I am working with STM32H753 and I am developing baremetal application using FMC. The FMC is interfaced with an external asynchronous memory, address and data signals are not muxed and there is no need for NWAIT, NADV nor CLK signals.On the FMC sid...

Pull-up required on NRST line?

Hello everybody,I am quite new from working with STM32 products but recently made the switch from Atmel chips (thanks to the free handout of Nucleo boards at the Eurobot competition I guess :) ). I recently designed a fairly simple board, centered ar...

Capture d’écran de 2023-07-02 21-17-59.png
felixzero by Associate II
  • 30943 Views
  • 11 replies
  • 3 kudos

Resolved! STM32L432KC basic DSP loop. Any way to improve this?

I am using Nucleo STM32 L432KC board with STM32CubeIDE v1.12.1 and doing very basic DSP operations with data values read via ADC through DMA into a circular buffer. It works, but the math is slower than expected.Below is an example loop in my code. A...

JBeal.1 by Associate II
  • 2804 Views
  • 3 replies
  • 4 kudos

STM32CUBE IDE STM32L152VBTx and WakeupCallback -- None?

Hello,I am moving code from one MCU to this old STM32L152 in where the UART is configured as Multiprocessor Mode.I am using STM32 CubeIDEI get compile error..   It looks to me like there is no WakeupCallback at all. HAL_UARTEx_WakeupCallbackHAL_UART_...

Eddiie by Associate II
  • 2733 Views
  • 4 replies
  • 0 kudos

STM32U5A5: OCTOSPI and 1.08V GPIOs

In datasheet for STM32U5Axx is mentioned:a) "up to 14 I/Os with independent supply down to 1.08 V" - cool, great feature I needb) OCTOSPIM: "efficient OCTOSPI pin assignment with a full I/O matrix (before alternate function map)"What does it mean?Cou...

tjaekel by Lead
  • 1167 Views
  • 1 replies
  • 0 kudos

Resolved! Use ADC with DMA, then DMA to SDIO/MMC?

Hi all,I am using a STM32H723ZG Nucleo-144 board. Here I have attached a micro-SD card module. I am sampling from one of the ADCs with 8.33 Msps at 8-bit resolution. I am able to transfer the data to RAM using DMA without any loss. However, I wonder ...

elso by Senior
  • 2035 Views
  • 2 replies
  • 2 kudos

CEC HDMI hanshaking example and bug in MX report

First bug, i start testing CEC on F051DISCO . Open MX create config for KEIL v5 and generate code.After build and load i spent some hours to locate why code dont receive and hangs. Elaborate bad generated startus assembler file where is IRQ named CEC...

MM..1 by Chief III
  • 1566 Views
  • 2 replies
  • 0 kudos

Resolved! DMAMUX configuration

Hello community,I cant get the dma working on the stm32g474. What I did till now:- enabled tim15 -> working with interrupts- enabled dma req. on update event- enabled dma and dmamux clocks in rcc- enabled dma int in nvic -> can be triggered through n...

Restart issue

Hi , I am using STM32L072CZT6 for our low power application. We are using Standby mode with RTC for alarm and periodic interrupt wakeup. The device is wakeup and work properly for more than 12 hours hours. After that the controller didn't operate and...

Deepu joy by Associate II
  • 3112 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.