STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! GPIO Usage on STM32N6

This is a pretty basic question but I would like a bit of clarity if possible.If a GPIO pin is configured for the fsbl code can it also be used in the Appli code?If so how would you go about defining it in the Appli code? There doesn't seem to be an ...

digilog by Associate II
  • 550 Views
  • 1 replies
  • 1 kudos

Regarding DCMI Data Reception Issues

Our company has a chip that outputs data via DCMI, though it does not employ a standard DCMI interface. It lacks a horizontal synchronisation signal, possessing only a vertical synchronisation signal. Could you advise which chips are capable of recei...

STM32L031C6 reading vdda & temperature

Hi,I have a custom board with an STM32L031C6 and I'm trying to read the internal temperature. The board is battery powered at about 2.6V and the vdda is the same.If I read the ADC channel with vrefint, it returns a value of about 850, which, when pas...

Ufoit by Associate II
  • 1114 Views
  • 7 replies
  • 0 kudos

Resolved! TIM1 PWM BK and BK2 strange behavior

Hello,I configured TIM1 as shown in the attached image: Everything works as expected I am controlling an inductive load which oscillates heavily after the PWM is turned off. I therefore decided to immediately short the low-side MOSFET (CH1N) to groun...

PKurz1_0-1764499214309.png PKurz1_1-1764500584419.png PKurz1_2-1764500870035.png PKurz1_3-1764500939017.png
PKurz.1 by Associate III
  • 621 Views
  • 2 replies
  • 1 kudos

New STM32F4xx Reference Manual RM0090

Posted on November 05, 2012 at 11:28Revision 2 of RM0090 is available. http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REFERENCE_MANUAL/DM00031020.pdf JW

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.