STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unusable STM32L01 MCU pins?

Hello, all.I'm trying to design and build my first STM32 project, a timer. I'm using the STM32L101K4 and have it configured as illustrated in the attached screenshot. The pins are configured in STM32CubeIDE as:External LSE on 2 & 3LCD connections on ...

KevinZ by Associate III
  • 6151 Views
  • 8 replies
  • 0 kudos

STM32F411 - common short questions ...

Good Evening Ladies and Gentlemen, A short introducing purpose of mine: int main(void) { RCC->AHB1ENR |= 0xFC; // ---> Here I would like to open the Port clock RCC->APB1ENR |= 0xFC; // ---> Here I would like to open the USART2...

timbo2023 by Associate III
  • 14339 Views
  • 35 replies
  • 3 kudos

GT911 stucks/freezes in multitouch.

Hello Community,I'm using GT911 with STM32F746 over I2C. I have noticed some time it stucks when multi touch is used (very few times in single touch as well). Upon debugging I noticed a change of voltage level of Interrupt pin.In working state, INT p...

0693W00000UnmnYQAR.jpg 0693W00000UnmpeQAB.jpg
KAgga.1 by Associate III
  • 3731 Views
  • 2 replies
  • 0 kudos

nRF24L01+ receiver problems

Hello,I am currently using a custom-built board designed to the nRF24L01+ specification and using the same exact circuit provided in their datasheet. It is connected to my STM32F103 through SPI. I am currently using this library to test out this boar...

Resolved! STM32L476 minimal ADC sampling time

Hello,STM32L476 data sheet Rev 8 talks in 3.15 about "Down to 18.75 ns sampling time" while table 77 only lists a minimal 31.25 ns minimal sampling time. Is 18.75 ns sampling time possible and with what setting?

Resolved! Read wrong content of MCU's internal flash

HelloI am working in dual bank mode with STM32G474RET6 MCU. I want to store some default values in internal flash beyond last programmed firmware's data address.For example I have following contents in flash (shown from STM32CubeProgrammer):Data star...

AlexHalf_0-1704730435486.png

Resolved! Getting problems with CAN on a NUCLEO-F207ZG Board

Hello everyone,   for a project I try to build a small CAN Bus with several Nucleo 144F207 Boards. Sadly, I have a really hard time to get it to work even though it should be rather simple. The minimum setup consists of two boards and two CAN Trancie...

CANconfig.PNG Scope1.jpg

Resolved! TSC Example

I am a begginer in the st enviroment, but still. I'm trying to use the touch sensing library, but there is very little good examples of how to just use one button as a sensor. I real all the documentation, still no good examples. I downloaded the lib...

mihaheh by Associate
  • 3093 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.