STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stlink v3 mini cannot program c031g4u6, Target no device found

i am sorry for creating a lot of post recently but i just can not program my microcontrollers. when ever i try to program it i get this:STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rights reserved. S...

WhatsApp Image 2024-01-11 at 22.24.12.jpeg WhatsApp Image 2024-01-11 at 21.59.11 (3).jpeg WhatsApp Image 2024-01-11 at 21.59.11 (2).jpeg WhatsApp Image 2024-01-11 at 21.59.11 (1).jpeg
oyalç.1 by Associate III
  • 8928 Views
  • 16 replies
  • 7 kudos

Single ADC Reading with Multiple DMA Channels

Hi,Is it possible to have a single ADC result transferred to two different memory locations using DMA without CPU intervention?Specifically I want DMA to take a single reading from an ADC, transfer it to one location on the STM32H747 CM4 and another ...

slc2015 by Associate II
  • 2249 Views
  • 3 replies
  • 0 kudos

STM32G491KCU6: Unable to program via UART1

Hello,I'm trying to program G491KCU6 board via UART1 and I'm not able to connect to st-programmer. I don't know whether the board is actually entering Boot0 or not. I have PB8 with 10K to GND and I pull it up during connection to enter Boot0. Below i...

MallikarjunSE_0-1705136656649.png

Trouble with SDRAM and STM32F469

Hi all!I am struggling to couple STM32F469ZGT6 (running at 180 MHz) with SDRAM type IS42S16160J-6TL from ISSI (datasheet here: https://www.issi.com/WW/pdf/42-45S83200J-16160J.pdf ).SDRAM is organized in 4 banks, each having 8192 rows x 512 columns x ...

ELowe_0-1704819258745.png ELowe_1-1704819258756.png ELowe_2-1704819258761.png
ELowe by Associate III
  • 3733 Views
  • 4 replies
  • 1 kudos

Resolved! L433 SDMMC FIFO doesn't get emptied

I'm currently working on a project using the STM32L433 MCU with the SD peripheral. While trying to use the HAL driver with read and write operations the functions return an timeout. While tracing the command and data lines the command is sent but the...

JSwildens_0-1704660275058.png

Resolved! Inquiry Regarding MCU with Specific Features

Dear STMicroelectronics Support Team, I hope this message finds you well. I am interested in identifying a microcontroller that meets certain specifications for my project. I would appreciate your assistance in identifying the most suitable MCU. MCU ...

pumarada by Associate III
  • 5359 Views
  • 9 replies
  • 2 kudos

Resolved! STM32 NUCLEO-L4A6ZG Resources and Examples

Hey,I'm completely new to the topic of microcontrollers and currently trying to prepare for an internship (preparation and prior knowledge are not required, but I would still like to prepare myself). Since I already the chip (STM32L4A6) I'm going to ...

stmax by Associate II
  • 6093 Views
  • 7 replies
  • 3 kudos

STM32G4: USART FIFO Error Flags

I'm using the USART on my STM32G474 in FIFO mode with LL-libraries. The datasheet says:" However the RXFIFO default width is 12 bits. This is due to the fact that the receiver does not only store the data in the FIFO, but also the error flags associa...

Herm by Associate III
  • 4025 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.