STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RS485 and Modbus

hi i am saishiva i am working on the STM board from 10 days but i am not getting the clarity about the how to activate the RS485 using the modbus protocol can you pleaae help on that  

saishiva by Associate
  • 1228 Views
  • 0 replies
  • 0 kudos

How to fix error return by SDMMC_GetCmdResp1

Dear Sir,I have interfaced SDHC card 32GB of Sandisk with STM32L452RET6 microcontroller SDMMC1 peripheral in mode - SD 4 bit wide bus. In my device SD card as a Datalogger.Issue - When my device is working mean data is logging (Data writing in SD car...

KPras.2 by Associate III
  • 2498 Views
  • 3 replies
  • 0 kudos

Resolved! MCU at 1V8 - a need for UART level shifters?

I saw on NUCLEO-U5A5 schematics - there is a level shifter for signal T_VCP_TX:a bit obvious: if MCU jumper is set to run on 1V8 VDD - an external UART receiver (e.g. CP2102N) would not get anymore correct UART_TX signals (yes, it does not anymore wi...

LS_1V8_UART.png
tjaekel by Lead
  • 3607 Views
  • 2 replies
  • 3 kudos

Resolved! STM32C0 SO8N bootloader: I2C and SWD

Hello,which interfaces does a virgin STM32C0 in SO8N offer on the first boot for programming? AN2606 says USART1 and I2C1. In other cases, AN2606 adds a note when SWD does not work, but no such note is there for STM32C0. So, I assume SWD is supported...

lukasl by Associate
  • 2612 Views
  • 2 replies
  • 3 kudos

Resolved! Boot Library

I'm using an STM32H745 and have developed the Boot code, which works as expected when built as part of an application.  However, having converted the Boot code to a static library and linked it into the same application the Boot startup section .isr_...

NBrick67 by Associate II
  • 1812 Views
  • 2 replies
  • 1 kudos

Can't erase/write some Flash page in STM32G071RB

Hello,I'm writing a Flash HAL driver in order to understand better how this CHIP work.My functions at the moment work correctly but for some page I have an HardFault(During erase).For example I can't erase/write the page 0 and others pages.Please cou...

dmrsim by Associate III
  • 2395 Views
  • 3 replies
  • 1 kudos

HID issue with multiple report id

Hi Everyone,I am currently using STM32F103 for making a usb hid which acts as both, a keyboard and a gamepad.Please take a look at the descriptor and code below.Both of these work properly when used individually but when I combine them both and add r...

aksh3101 by Associate
  • 4831 Views
  • 3 replies
  • 0 kudos

ExT interrupt not firing.

we are using EXTI1 interrupt in our project based on stm32f446. But the Interrupt handler is not firing.We looked into the interrupt enable registers, Mask registers, etc and all seems fine and a timer interrupt also in the project, which is triggeri...

KumarTP by Associate III
  • 3767 Views
  • 4 replies
  • 4 kudos

Resolved! Avoid cross-effects between the LC sensors

Hi all,I'm using application note AN4636 for LC sensor.I tested with the example source code, and they work well for one sensor.But when I use multiple sensors, I face an issue. If I use the same value for inductor and capacitor for each sensor, the ...

phoungvd by Associate II
  • 4754 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.