2016-12-13 6:09 PM
I noticed the function description of the PI_GetDefaultKI and the PI_GetKI are same in FW API description. What is the difference between them?
I can't understand PI_
SetIntegralTerm. the description is so vague.
Can someone explain something , please?
thanks.
#library #foc-mdk-4.32021-06-15 12:21 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.