STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! EVLSERVO1 Over Current Protection (OCP)

Hello everyone,Based on the screenshots attached, I couldn't understand the formula obtained for the OCP feature of this inverter board.3 phase currents are read through the shunt resistors, got offset, and amplified by the op-amp ICs. So far so good...

Resolved! How to limit Iq current?

Hello Everybody, MCSDK:6.3.0 CubeMX: 6.3.0 Workbench : 6.3.0 Motor Pilot : 1.2.9 Power Board : IHM08M1(Rshunt=0.01Ω) Control Board : NUCLEO-G431RB Motor : BLDC 26w 24v/8 pole pairs / rpm=4k / rated current=1.8A/hall sensor   I would like to ask, in S...

Vincent7 by Associate III
  • 2121 Views
  • 1 replies
  • 1 kudos

How do you reset the motor control system?

I am working on a system that the on/off button only switches the high-voltage power source.  The processor and IPM continue to run.  First problem we had was that you cannot clear faults or execute the MC_StopMotor1() function because the system is ...

B-G431B-ESC1 can't connect to Motor Profiler

 Hey, I have troubles with my B-G431.Two problems with the B-G431:MotorProfiler 5.4.8: Measurement of Profile is taking too long, no matter how I change the values. MotorProfiler 6.3.2: Can't connect to the Board. It can't even open the port. Does an...

orka375_0-1741011916269.png orka375_1-1741012160722.png orka375_2-1741012315304.png
orka375 by Associate
  • 987 Views
  • 1 replies
  • 0 kudos

Resolved! SDK6.3.2 completed with error

 Hi, Partner,Here's the problem I've encountered and how to solve it,I'm working with the following setup:System: win 10 22H2, RAM 4G, i3-6100 Hardware: Nucleo F072 + STEVAL - IPM03B +SPMSM 0.8HP + Hall sensorSoftware: SDK6.3.2, Cube Max 6.13, Cube I...

walen_0-1741232130261.png walen_0-1741233581851.png walen_1-1741233729764.png
walen by Associate III
  • 2080 Views
  • 4 replies
  • 0 kudos

MCSDK - 6.3.2 PWM pin order

I have a custom design using SDK 6.3.2 that was started by modifying the board files from NUCLEO-L476RG and X-NUCLEO-IHM07M1. When the custom board was designed, the Phase order was changed from default (U/W flipped):TIM1_CH3/3N, ADC1_IN1 Current - P...

jzach_0-1741307754957.jpeg
jzach by Associate
  • 677 Views
  • 0 replies
  • 0 kudos

Resolved! ACIM support - which version to use?

On the wiki page:https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor It says:""This article applies to the 5.Y.* versions series of the X-CUBE-MCSDK. ACIM motors are not supported in older versions of the X-CUBE-MCSDK (v5.4.* a...

lamare by Associate III
  • 1190 Views
  • 1 replies
  • 0 kudos

Injected ADC on PWM timer (Timer1)

Hello community Please help me, i am facing issue related to injected ADC on PWM timerMCU : stm32f103, working on motor control for BLDC motorExcepted : When motor is running that means it generated PWM, at that time Injected ADC value must be shore....

snehadakhare01_0-1741257626872.png snehadakhare01_1-1741257644532.png snehadakhare01_2-1741257660108.png snehadakhare01_3-1741257673470.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.