STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

St motor workbench CubeMx error

Hi everyone,I have problem about ST Motor Control Workbench.I can ' t generate project.I tried so many things(I installed and unistalled different versions , I changed OS language etc.) but I couldn't do it .Please help.

stPic.PNG
ilker07 by Associate III
  • 8794 Views
  • 25 replies
  • 1 kudos

STSPIN32F0A OC protection

Hi, I'm using STSPIN32F0A to control BLDC.I have a question regarding the operation of the OC protection.we expected that the two corresponding low side MOSFETs would turn on when OC COMP pin detects the over current.However during actual operation, ...

Ryo1 by Associate
  • 974 Views
  • 1 replies
  • 0 kudos

STEVAL-CTM012V1

I have STEVAL-CTM012V1 evaluation board for 250 W. I have followed all the procedure which are mention in the manual where I first load the firmware file stsw-ctm11 in motor control work bench then click on generate code then goes into cubemx then ge...

Resolved! STMicroelectronics STEVAL-CTM015V1

Hi everyone, I have purchased a STMicroelectronics STEVAL-CTM015V1 drive. How can I find its default firmware code (Current chopping control for switched reluctance motor) in  STM32CubeIDE workspace? I would like to get connected with the people alre...

STSPINF0251 Not spinning BLDC motor

Hello,We've designed a STSPIN32F0251-based motor driver board, but when running the 6-step firmware algorithm, the motor aligns and then vibrates with a high-pitched sound. When we check the state-machine, we can see it reaches the RUN state after ex...

kenni_4-1741042639147.png kenni_5-1741042696150.png
kenni by Associate II
  • 1129 Views
  • 0 replies
  • 0 kudos

Rev-up and stop ramps

How can I change the rev-up and stop ramps programatically ?I can change the rev-up ramp through motor pilot but I have to do it everytime it connects.I want to control that through the program.I'm using code generated from the MC WB / MC MX / MX IDE...

B-G431B-ESC1 Board not working properly

I am using B-G431B-ESC1 board and GBM2804H-100T Brushless Gimbal Motor, properly generated the code. But upon receiving PWM signal, Motor is behaving:Motor spins then zero spins then zero soon then spins.Although Motor is working with other controlle...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.