STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

High sensitivity observer mode

Hello,I am an employee of a company producing underwater scooters, currently working on implementing the STSPIN32G4 microcontroller in our products. I have the following question:In the Motor control Workbench software, in the "Speed ​​Sensing Mode S...

calka by Associate II
  • 3174 Views
  • 4 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

IHM16M1 and G474RE

i am trying to use the IHM16M1 with the NUCLEO-G474RE.  i have it plugged into the top of the Nucleo board via the Morphio connectors.I can supply power (12v) to the IHM16M1, but it does not seem to be powering the G474RE.I have tried JP5 on the Nucl...

EVALSTDRIVE101 project file

Good day, I am wondering there is a way to access the project file for the EVALSTDRIVE101 demonstration board. I need to do a custom board based on it and only the Gerber files are available. I would appreciate any help. Thanks in advance  Mostafa   

Resolved! EVLSPIN32G0A1: Issue with compiling code

Hi,I got several FreeMarker template errors when I tried to compile the code to test out EVLSPIN32G0A1. It looks like all the files under MotorControl folder were affected by what I assume is the same error type (see attached picture).FreeMarker temp...

STMCubeIDE_Error.png
Bam by Associate II
  • 4693 Views
  • 8 replies
  • 0 kudos

Resolved! Error during generating project

Unable to generate motor control project using MCSDK 6.3.2The MCU is STM32G473CCU6"It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the fol...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.